Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Change relation type during export PDF from NX in Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon,

When drawings are exported as a PDF (NX: File -> Export -> PDF ...) then it gets added as dataset under item revision with relation IMAN_manifestation.
How can this behavior be changed? It is necessary that the PDF dataset is added with the IMAN_specification relation. When exporting from NX, I did not find any settings that allow me to change the relationship type.

2 REPLIES 2

Re: Change relation type during export PDF from NX in Teamcenter

Legend
Legend

I think I have found solution - check the NX customer defaults - go to the Export PDF settings->Teamcenter Integration. There is first option - relation for dataset creation. There are 2 options there, try first

 

1111.JPG

Re: Change relation type during export PDF from NX in Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, thanks for the tip! It works!