05-23-2018 05:38 PM
Good afternoon,
When drawings are exported as a PDF (NX: File -> Export -> PDF ...) then it gets added as dataset under item revision with relation IMAN_manifestation.
How can this behavior be changed? It is necessary that the PDF dataset is added with the IMAN_specification relation. When exporting from NX, I did not find any settings that allow me to change the relationship type.
Solved! Go to Solution.
05-24-2018 02:33 AM - edited 05-24-2018 02:39 AM
I think I have found solution - check the NX customer defaults - go to the Export PDF settings->Teamcenter Integration. There is first option - relation for dataset creation. There are 2 options there, try first
05-24-2018 02:03 PM
Good afternoon, thanks for the tip! It works!