Cancel
Showing results for 
Search instead for 
Did you mean: 

Changing icon / button size in TC

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

 

 

Hi, all

 

Working on site at a customer and recently they've started replacing monitors with 4k....

Fine for NX, but TC is obviously not yet 4k ready.

Biggest problem at the moment is the size of the icons / buttons, and the way that some things display when its at high res...

 

This is the most important bit...

 

tc_small_icons.png

 

Also the Edit > Options menu is up the spout

 

I've got it in my head that the sizes of these buttons can't be changed but I'm hoping someone can tell me different? Cheers.

 

1 REPLY 1

Re: Changing icon / button size in TC

Gears Phenom Gears Phenom
Gears Phenom