Cancel
Showing results for 
Search instead for 
Did you mean: 

Check-In/-Out function greyed out?

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

 Dear Community,

 

iam facing a  strange phenomenon with the check in/out function in TC.

 

If i check out an Dataset (explicit) and check it in again the functiion is greyed out...If i do it implicit (e.g. CAM...) it works....

 

If i set an null (0) value to the preference TC_checkout_and_export it works also fine (without export of the physical file)....

 

Version (Tc): 11.4.0.5 (+PLM Easy)

 

What else was i missing?

 

Thank you guys... have a good start in the new working week !!

 

BR Luke