Cancel
Showing results for 
Search instead for 
Did you mean: 

Check in data sets?

Gears Phenom Gears Phenom
Gears Phenom

Tc 10.1.2

 

Is there a command the Tc admin can set to run at some interval, that will check in data sets that have been kept checked out for some unknown reason (NX crash, etc)?  Obviously we wouldn't want it checking stuff in that was still being worked on, but maybe things left checked out for more than X number of days or something?

-Dave
NX 11 | Teamcenter 11 | Windows 10
7 REPLIES

Re: Check in data sets?

Valued Contributor
Valued Contributor

Dave,

I am not aware of such a utility (but I may be wrong)

I set up a checked out objects search for all my users, and chase them up to make sure they run it at least once a week.

 

2015-12-11_14-49-58.jpg

Re: Check in data sets?

Gears Phenom Gears Phenom
Gears Phenom

Thanks, that doesn't remove the human element, but is better than we have now!

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Check in data sets?

Valued Contributor
Valued Contributor
Dave,
There is no OOTB utility for that purpose available.
We built an ITK Program for checking in checkedout Workspace Objects. This is run through a ScheduledTask daily at night.
Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP04 + TC10.1.7.1
Testing: NX11.0.2.7 MP11 + TC11.5.0.4
Unstable: NX12.0.2.9 MP03
Development: C#

Re: Check in data sets?

Gears Phenom Gears Phenom
Gears Phenom

Thanks.  I doubt custom code is an option, unless we outsource it.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Check in data sets?

Valued Contributor
Valued Contributor

This is not exactly what you're looking for but this helps us quite a bit in the above mentioned issues.

Set the TC Option TC_show_checkout_objects_on_exit this will give the user a list with all checked out objects when logging out of TC. And here the user can also check in the files.

 

-Jelle-

 

Re: Check in data sets?

Experimenter
Experimenter

Have you implemented this? If so was it successful?

Re: Check in data sets?

Valued Contributor
Valued Contributor

Yes, and yes it is a great tool. I highly recomend it from an administrators point of view.