Cancel
Showing results for 
Search instead for 
Did you mean: 

Classic variants in TC11.2.3

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi

I'm running VM TC11.2.3 and want to do classic variants in structure manager but it is missing from the data panel.

 Variants_data_panel.jpgdata_panel

 /Peter

4 REPLIES 4

Re: Classic variants in TC11.2.3

Select a BOM line in Structure Manager and then select Show/Hide data PaneCapture.PNG

Re: Classic variants in TC11.2.3

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I think I see a 'Variants' view tucked next to 'process history'...so the variant features you are looking for is already in your workspace. 

 

Harish

Re: Classic variants in TC11.2.3

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

I have found the answer. When product configurator is installed the preference "PSM_enable_product_configurator" is set to "true" which somehow disables classic variants.

Setting it to "false" will show the variants tab in the data panel in structure manager again after a restart.

Re: Classic variants in TC11.2.3

Experimenter
Experimenter

Thanks, that is the solution in my case where I installed Product configurator module.