Cancel
Showing results for 
Search instead for 
Did you mean: 

Clear organization of all groups and replace it with the default

Experimenter
Experimenter

Hello,

 

Is there any way to overwrite  the  current organization and replace it with the teamcenter default?

4 REPLIES

Re: Clear organization of all groups and replace it with the default

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The Organization is foundational to the entire environment and has too many dependencies to be simply replaced. It affects ACL's, Change Management, Workflows, PAL's/Dynamic Participants, Workflow Filtering and a whole mess of other functionality that is spread across Teamcenter and BMIDE.

Short answer is: No. A longer answer is, yes, but it will take significant resources to redesign/align/deploy. The long answer requires you to install Teamcenter with the default Org in a separate environment then migrate the current content to the new environment while mapping one to the other. Not a option for the faint of heart (hence the short answer). Warning: migrations are ALWAYS messy things.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Clear organization of all groups and replace it with the default

Valued Contributor
Valued Contributor

Why do you want to do that?  It's more or less like starting over.

Re: Clear organization of all groups and replace it with the default

Experimenter
Experimenter

i'm working on a test server and was wondering if I can overwrite from TC command the Organization without renaming manually(from rich client) the Groups.

Re: Clear organization of all groups and replace it with the default

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You would need to provide the UID of the group and I can't think of any utils to do this right now (probably is a way but my head cold has me a bit fuzzy today). The easiest way I can think of is using SQL commands directly against the DB. However, you are unsupported in that activity. The PUID is the key to changing the name.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4