Cancel
Showing results for 
Search instead for 
Did you mean: 

Client Cache issue

Genius
Genius

Hello;

 

Recentely I get a message when some users want to login to clien. the message is:

"The client cache is empty. The rich client is logged in in skip cache mode. If you wish to improve Rich Client performance see your administrator about generating a client cache."

 

I don't know what is the issue. Anyone know about what to do?

 

Thanks.

BR.

8 REPLIES 8

Re: Client Cache issue

Legend
Legend

generate the client cache using the command below.

generate_client_meta_cache -u=infodba -p=password -g=dba generate all

 

this will remove warning currently display during login

Re: Client Cache issue

Pioneer
Pioneer

Hi Guys,

 

Do i need to go to Teamcenter directory to do the following command ?

Still new to this application and i facing the same issue.

Can provide any sample, thanks.

 

Steven

Re: Client Cache issue

Creator
Creator
Hi,

You have to run this command on the application server in a TC Command prompt.
---------------------------
Björn Andersson
Solution Architect
PLM @ Nibe AB

---------------------------

Re: Client Cache issue

Siemens Creator Siemens Creator
Siemens Creator

Hi BKA,

 

I absolutely met the same issue and I tried taking your suggestion and it works for me now. However, I am kind of interested in how come this could happen.

 

we deployed something through BMIDE recently and after that this issue arose.

 

looking forward to your reply. Thanks!

Re: Client Cache issue

Genius
Genius

@Mason

Hello;

It could happen due to many reasons, but it your case it seems that when you deployed your template you forgot to select "Create_client_cache" option. anyway what you have done is the same thing but manual.

 

BR.

Re: Client Cache issue

Siemens Creator Siemens Creator
Siemens Creator
OK. I will keep my eye on it next time when I deploy. Thanks!

Re: Client Cache issue

Gears Phenom Gears Phenom
Gears Phenom

@JFK1963 - I've had an instance that said it updated the client cache when I deployed but it absolutely didn't do it. I read the logs and it said the commands completed successfully. It didn't. I would have to do it manually after each time I deployed. It was weird. So why it happens is sometimes a mystery.

 

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Client Cache issue

Genius
Genius

@Jamie_Griffis

ah I understand, it can happen due to many reasons. the command for sure comes in handy...