Cancel
Showing results for 
Search instead for 
Did you mean: 

Cold Deployment error

Hello Team,

I am facing below issue while deploying package extension.

 

Executing ["C:\Siemens\TC101\bin\manage_model_files.exe" -u=infodba -p=***** -g=dba -force=model -option=download]
Output from command: "C:\Siemens\TC101\bin\manage_model_files.exe" -u=infodba -p=***** -g=dba -force=model -option=download
Downloading File: model.xml
3072: The FTS engine could not be found.
41178: FSC proxy error: "6 CURLE_COULDNT_RESOLVE_HOST: The host domain name to which you are trying to connect could not be resolved.".
command_exit=41178
Exit Status 41178, elapsed time 0:01:44
An error occurred during execution. Stack trace follows...
com.teamcenter.install.tceng.base.DatabaseSteps.manageModelFiles(DatabaseSteps.java:3039)
com.teamcenter.install.tceng.base.DatabaseSteps.updateDatabaseAll(DatabaseSteps.java:2766)
com.teamcenter.install.tceng.base.DatabaseSteps.updateDatabase(DatabaseSteps.java:2728)
sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
java.lang.reflect.Method.invoke(Unknown Source)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:209)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:135)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1350)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1288)
com.teamcenter.install.tem.struct.TcFeature.maintenance(TcFeature.java:1048)
com.teamcenter.install.tem.director.actions.MaintenanceAction.execute(MaintenanceAction.java:30)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:143)
com.teamcenter.install.tem.director.Director.run(Director.java:120)
java.lang.Thread.run(Unknown Source)
com.teamcenter.install.tem.struct.exceptions.UserCancellationException: User cancelled

5 REPLIES 5

Re: Cold Deployment error

It was due to preferences, I have directly imported all the site preferences from the development environment to production environment. in which some preferences are having Host names and those preferences should not override such as

Fms_BootStrap_Urls
Transient_Volume_Installation_Location
Default_Transient_Server

so after restoring the preferences, this issue got resolved.

Re: Cold Deployment error

Experimenter
Experimenter

How did you restore the preferences?

Re: Cold Deployment error

Valued Contributor
Valued Contributor

I am facing similar issue.

I created DEV environment from fresh install. Once features are installed, I did TEM --> Manage Admin Data --> Import Admin Data, from the package that I exported from PROD environment. Without realizing key preferences, I just overrided all preferences. 

So obviously, I faced FSC error while uploading any files to TC. 

 

Later, I restored preferences by running preference_manager, restoring all site preferences back to original DEV Preference values. Still, am getting this error, while logging into Teamcenter 2 Tier Client.

 ERROR 41178 FSC proxy error: "-9009 NO_ROUTE_3{<SITE-ID>}{volume/logvolume}{<VOLUME-ID>}".

 

Any idea?

 

Thanks,
Anbu

Teamcenter Architect & PLM/CAD Administrator,
Teamcenter 11.4 | Active Workspace 3.4 | NX 12

Re: Cold Deployment error

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Check these preferences:
Fms_BootStrap_Urls
Default_Transient_server
Default_Transient_Volume_Id
Transient_Volume_Installation_Location
Transient_Volume_RootDir

Compare results from backup_xmlinfo with FMS Master and the above prefs.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Cold Deployment error

Valued Contributor
Valued Contributor

Thanks, after updating the preferences, it works fine!

Thanks,
Anbu

Teamcenter Architect & PLM/CAD Administrator,
Teamcenter 11.4 | Active Workspace 3.4 | NX 12