Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Compatibility of TC & Office

Builder
Builder
Dear all,
I want to know if teamcenter 8.3 Office 2010 and Windows 7 are compatible with each other.
Sina Shojaee
4 REPLIES 4

Re: Compatibility of TC & Office

Genius
Genius

 

I know they are compatible as we used to have the similar setup a while back. But, we were on 8.3.3.8 and  you will have to meddle with the registry settings on the RAC as the icons are not visible in MS office products. There is a solution for this on the GTAC Solution Database.

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Compatibility of TC & Office

Valued Contributor
Valued Contributor

Hi,

 

I would like to join the discussion with the questions if, Teamcenter 11.2.2 is compatible (the "Viewer" integration) with:

 

- Office 365 in general

- Office 2016

 

Thanks & br

Julian

Re: Compatibility of TC & Office

Genius
Genius

Jul...were you able to get this answered?  I am curious about this myself.  We're running 10.1.x, but our Office was recently upgraded to 2016 and we are having all kinds of trouble.

Re: Compatibility of TC & Office

Genius
Genius

See here