Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Control Axis in kinematic operation in Teamcenter

Experimenter
Experimenter

Is there any possibility like in Nx to control the axis of cnc machine to control the movement of tool tip in Teamcenter, for example i want to bring the tool tip to the specific point.

is it possible or no. please guide me?

3 REPLIES 3

Re: Control Axis in kinematic operation in Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Where do you want to do this?

 

NX has its own dialog, which you don't have access in Tc.

In Tc you would use regular movement of assembly components.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Control Axis in kinematic operation in Teamcenter

Experimenter
Experimenter

My promblem is that when i use custome assembly operation by kinemtic assembly operation. i couldn't stop the machine. i applied kinematic and custom assembly operation in order to move the 3 axis cnc machine but actually when i run the simulation there is no possibility to stop the the tool tip in a specific position like in Nx.

To make it clear. i want to know that how can i tell to the tool tip to go to the specific point in the teamcenter visualization? is it possible or no.?

Re: Control Axis in kinematic operation in Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

TcVis is only a part and assembly viewer, it is not an IS&V viewer.

If you need this, you will have to install NX.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide