Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Properties BMIDE

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hello Everyone,

How do you attribute names to your properties in BMIDE to have a default and to be able to find these properties after, to modify?

Thx!
1 REPLY

Re: Create Properties BMIDE

Legend
Legend

Hello,

 

Default value for each property in BMIDE can be set in two ways

 

Class level: This can be set when creating a persistent property on a business object. Set the initial value field in the 'Add Attribute' popup window

 

Business Object: Default value can also be set using the 'Initial Value' property constant available while a property on a business object is selected

 

Setting the initial value property constant is quite simple and easily modified later when required.

 

Regards,

Mahendra