Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating 3D datas to share on Internet automatically from TEAMCENTER

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

One of our prospects for TC Rapid Start is asking this.

They want to add STEP or PARASOLID models to their products on their website.

They want the weight, material and 3D data(that anyone would like to download from the link) to be accurate as a designer could change anything on Teamcenter.

Can a live link like this be done between TC and their website?

 

Cem

4 REPLIES 4

Re: Creating 3D datas to share on Internet automatically from TEAMCENTER

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

You can use Tc to integrate with SharePoint and expose that to the outside world. However, you will still need user accounts for anyone viewing the info.

 

There is a new product being created called Linked Data Format (LDF) that will be released soon or is released with Tc11.2. The LDF model will allow a "service" user to connect so special licensing is required.

 

I haven't implemented either of these so you'll have to do your own research.

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Creating 3D datas to share on Internet automatically from TEAMCENTER

Creator
Creator

Hi Randy

I was looking for the steps involved to integrate TC with sharepoint, Is it possible to integrate without Community Collaboration?
Can you please provide details for integrating TC with SharePoint.

 

Regards,

Gautam Ramini

Re: Creating 3D datas to share on Internet automatically from TEAMCENTER

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

I'm not a SharePoint expert (and don't want to be). Community Collaboration is a plugin for SharePoint and is the only ootb method I know of. Customization of SharePoint is beyond my skillset (by choice).

 

You can either investigate LDF (main stream method) or you can roll your own solution which will likely require coding in both Teamcenter and SharePoint. I can start you down that road by pointing you to a workflow action handler called EPM-run-external-command (old school method).


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Creating 3D datas to share on Internet automatically from TEAMCENTER

Creator
Creator
Ok, will check regarding LDF and also explore the customization.
Thanks!