Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating Folder under item revision.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello all ,

 

I need a help for creating automatically folder under the item revision while creating an a costum item . I can achive that , when i create a custom item and assaign id and name the folder is created under the item . But it takes a name from the item name. I want to give that folder a constant name such as "Material Documents" .And also i want to create a folder under the item revison not under the item. How can i do that ?

2019-01-25_11h14_21.png2019-01-25_11h15_27.png

 

Best Regards

Gurkan

2 REPLIES 2

Re: Creating Folder under item revision.

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, look at using the createObjects extension, try using it with Folder and IMAN_reference arguments

 

https://docs.plm.automation.siemens.com/tdoc/tc/11.6/help/#uid:id1673822

Re: Creating Folder under item revision.

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Or create a relation and "show" that relation as a pseudo-folder. Or create an IRDC.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4