Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a workflow to translate JT's from UGMASTER datasets

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

I tried to create a workflow to create 3D JT data from UGMASTER datasets.

Here are the screenshots from workflow designer.

1.jpg

 

2.jpg

 

I can create JT's with translate option in the Rich Client, but this workflow did nothing.

 

Is there something else I need to do?

 

Cem

15 REPLIES

Re: Creating a workflow to translate JT's from UGMASTER datasets

Creator
Creator

I would request you to check if translator services are started. If still you dont get then restart your client and also the translation services. If they are not automatically started.

 

Regards,

chini

Re: Creating a workflow to translate JT's from UGMASTER datasets

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Did both, did not work.

 

Do you think there is a mistake?

 

Cem ALPAY

Re: Creating a workflow to translate JT's from UGMASTER datasets

Creator
Creator

There is a typing error its ProviderName not providername.

 

Try this

Regards,

Chini

Re: Creating a workflow to translate JT's from UGMASTER datasets

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

3.jpg

 

This also gives the same output.

Re: Creating a workflow to translate JT's from UGMASTER datasets

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

please whether dispacther request has been created for this or not using Translate ->Admin console ?

 

If not there might issue related to dispatcher triggers.

Re: Creating a workflow to translate JT's from UGMASTER datasets

Creator
Creator

As best practice the dispatcher services are started in this order:

Dispatcher Module -> Dispatcher Scheduler -> Dispatcher client

 

When working with workflow, check if you can set debug key and track the tasks. by start use EPM-attach-related-objects and collect UGMASTER as target into the workflow. if you are starting workflow with ItemRevision or EPM-attach-assembly-components define 'depth'.

 

Try this.

 

Regards,

Chini

Re: Creating a workflow to translate JT's from UGMASTER datasets

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Dispatcher server, module and client are started in correct order.

Should I create the workflow like this?

2.jpg

 

This still didn't work.

 

Also it does not trigger any event, nothing in the administration console.

 

Cem

Re: Creating a workflow to translate JT's from UGMASTER datasets

Creator
Creator

Hello,

 

Here the relation is given wrong: In details view see the relation name may be specification.

 

For real name go to options->UI->Sys Admin-> Real Property Name

 

If needed check bmIDE for real property name. for this it must be

-relation  IMAN_specification

-att_type  target

 

 

Re: Creating a workflow to translate JT's from UGMASTER datasets

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Now the workflow is like this.

1.jpg

 

I right-click a UGMASTER and start this workflow

and get this error.

2.jpg