Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom Plugins not loading in 4 Tier

Experimenter
Experimenter

Custom plugins seems to be not loading in 4 Tier eventhough it is loading fine in 2 Tier.

 

Placed the plugins in TCROOT/portal/plugins folder and ran the registry.

 

After launching the 4T Client, not able to see the custom menu.

 

The same works fine in 2 Tier.

 

Any suggestions ?

 

TC 9.1.3.4

 

Thanks.

1 REPLY

Re: Custom Plugins not loading in 4 Tier

Experimenter
Experimenter

Issue resolved.

 

I didn't include the additional features such as SE, RM etc.. due to which the respective plugins were not available in plugins folder.

 

After installing those features, custom plugins loaded fine without issues.

 

Thanks.