Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Pioneer
Pioneer

Hi Expert,

 

I tried using below line in properties file but it is not working.

 

release_statuses.Obsolete.ICON=images/ACME4ff0000circle.png

 

Thanks,

Indrajeet

Highlighted

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Legend
Legend

Hi @Indra

 

If you want to append status next to Item revision, you can try

 

release_status_list.Obsolete.ICON=images/ACME4ff0000circle.png

 

Clear RAC cache and run genregxml.bat to see the changes.

Regards
Rafa

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Pioneer
Pioneer

Appending status next to Item revision is working fine but i want add under Item Revision.

Thank you Rafa for attention.

Regards,

Indra

 

 

 

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Legend
Legend

@Indra

 

You have to create a property render in BMIDE to append the status under the Item revision

 

I have attached you the document how to get it worked.

 

Regards
Rafa

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi

 

I am using TC11.5 version. For me the Release status without spaces are getting picked up from the customer.properties file. However, the ones with spaces are not working. I am using "\" for the spaces

 

release_status_list.L5\-\Baseline.ICO=images/ALI5_StatusRed.png
release_statuses.L5\-\Baseline.ICO=images/ALI5_StatusRed.png

 

The one which is working is:

release_status_list.Released.ICON=images/ALI5_StatusGreen.png
release_statuses.Released.ICON=images/ALI5_StatusGreen.png

 

Can you please help ?

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

You didn't provide a picture of your release status names in BMIDE so I can only go off of what your text says. Assuming that "L5 Baseline" is the display name (not the real name) of the status then...

 

This:

release_status_list.L5\-\Baseline.ICO=images/ALI5_StatusRed.png
release_statuses.L5\-\Baseline.ICO=images/ALI5_StatusRed.png

 

Becomes this:

release_status_list.L5\ Baseline.ICON=images/ALI5_StatusRed.png
release_statuses.L5\ Baseline.ICON=images/ALI5_StatusRed.png

 

My presentation from 2016 is attached.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Pioneer
Pioneer

Thank you so much for sharing the good info.

I will try this.

 

Thanks,

Indra

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Pioneer
Pioneer

Hi RandyEllsworth,

 

Hope you are doing Good!

 

Sorry for  the late reply , here is the attched staus list which we are using.

Note: all status in the list having same real and Display name.

 

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you Randy. I will try it out.

Re: Custom Release Status Icon does not render in Tc 11.4 RAC ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi 

 

I tried out the way as described in your ppt. I am able to get the flag against the item revision.

However, I want to change the flag of the status. It still comes black. TC 11.5.2

 

Icons are 16 x 16 pixel

 

customer.properties entry is:

 

release_status_list.Released.ICON=images/ALI5_StatusGreen.png
release_statuses.Released.ICON=images/ALI5_StatusGreen.png

 

BMIDE_Img.png

 


TC_Img.png

 

I have regenerated the cache. I have run the genregxml.bat.

But the flag of the Released as given in the screenshot is appearing black not the custom.

 

 

Can you please suggest ?

 

Ambuj