Cancel
Showing results for 
Search instead for 
Did you mean: 

Customize the "new Custom Item" create dialog

Experimenter
Experimenter

How to add one of the revision compound property on new Custom Item create dialog.

4 REPLIES

Re: Customize the "new Custom Item" create dialog

Phenom
Phenom

Hello, look in the documentation: Modify the item create panels in the New Business Object wizard using style sheets
https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help#uid:id738554

Re: Customize the "new Custom Item" create dialog

Experimenter
Experimenter
Thanks for quick reply.
I have tried all the options in the given documentation but it is not working.
Need to add one of the compound property of custom item in BMIDE Operation descriptor -> Create Input, how to add compound property in operation descriptor ?, after adding the required compound property only we can customize the stylesheet.

Re: Customize the "new Custom Item" create dialog

Phenom
Phenom

Where from do you get the compound property?

Re: Customize the "new Custom Item" create dialog

Phenom
Phenom

According to the documentation compound properties are not supported https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help#uid:xid1256815:index_plm00071:id166856:x...

Try the following:
1) Add your properties to the Operation descriptor -> Create Input in the revision of your business object
2) In the ItemCreate.xml of your business object, add the rendering of your properties

<section title="My Item Revision Properties" titleKey="tc_xrt_MyItemRevisionProperties" initialstate ="collapsed">
<property name="revision:my_prop_real_name_1"/>
<property name="revision:my_prop_real_name_2"/>
<property name="revision:my_prop_real_name_N"/>
</section>