Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Customizing the "Getting Started" application

Valued Contributor
Valued Contributor

Has anyone customized their "Getting Started" application in teamcenter? Or know if this is even possible?  I just want to add a few reference links for the rest of the engineering team.

 

any input is appreciated.

 

Thanks all,

Jake
4 REPLIES 4

Re: Customizing the "Getting Started" application

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I don't believe you can edit the "Getting Started" display, but it's possible to configure your client to display a different web site entirely. For example, you can display a page from your corporate intranet. The information about how to do it is available on the GTAC site; search for "myTeamCenterApp.URL".

 

Alternatively, you could look into using the LaunchPad perspective, which is hidden by default.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: Customizing the "Getting Started" application

Experimenter
Experimenter

Hi,

 

I already have a .html file ready. I would like this page to start with Teamcenter, rather than "Getting Started".
Which file or variable should I configure for this to work?

 

 

Tks!

Re: Customizing the "Getting Started" application

Valued Contributor
Valued Contributor

Hi @HelpDeskNemak,

 

For each client, in the "customer.properties" file located in the %TC_ROOT%/portal/plugins/configuration_*version* directory.  Add a line "myTeamCenterApp.URL=file://(location of your htm file)"

 

If  you do not have a customer.properties file in that directory I believe you can create it.

 

I recommend putting your htm file in a shared location where all clients can have a clear path pointed to it.

 

I am unware if this can be done at a site level or of any alternative methods.

 

Thanks.

Jake

Re: Customizing the "Getting Started" application

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Note: Always run genregxml.bat after modifying/adding/removing files in the plugins directory.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4