Cancel
Showing results for 
Search instead for 
Did you mean: 

Daily query to scan each user's inbox

Hallo everybody

 

I'd like to setup an automatic daily query to scan each user's inbox and then output, if present, the number of tasks to perform.

After that I'd like to export to OS such informations.

The aim is to daily notify by email users of the number of tasks they have to perform, as a remainder.

 

Thanks

Stefano Garbin
CAD & CAE manager
www.campagnolo.com
1 REPLY

Re: Daily query to scan each user's inbox

Genius
Genius

Stefano,

 

If your intention is to notify the user, that the task is pending. You could use an workflow handler EPM-late-Notification, to trigger an e-mail the the user, that the task is late. (Kind of a reminder).

 

For which you have to install the Task Manager Daemon to trigger this. Here is the link for the more info:

 

https://support.industrysoftware.automation.siemens.com/docs/teamcenter/10.1.3/help/#uid:index_workf...

 

Hope this helps !

Cheers.

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |