Cancel
Showing results for 
Search instead for 
Did you mean: 

Data model broken after update from Teamcneter 11.2.3p1 to 11.3.0

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hey,

Simple upgrade TC11.2.3patch1 to 11.3.0

1. MSSQL to simple recovery mode.

2. All tc services down.

3. TC11.3.0_install.zip unzip to istall directory with overwrite files.

4. Update manager and sucessfull patch of server.

5. Update BMIDE on another VM and (TC11.3.0_install -> update manager)

6. Load old datamodel to new BMIDE (updated and loaded without any errors).

7. Save and deploy.

8. When I want to make a full update I got this message:

2017-06-07_15h19_49.pngmark!

Is there a way to fix this?

3 REPLIES

Re: Data model broken after update from Teamcneter 11.2.3p1 to 11.3.0

Phenom
Phenom
any errors in console.log in the <BMIDE Proejct folder>\output ?

Re: Data model broken after update from Teamcneter 11.2.3p1 to 11.3.0

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

No errors.

BMIDE (after update to 11.3.0) load the project as usualy. 

 

Re: Data model broken after update from Teamcneter 11.2.3p1 to 11.3.0

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Problem solved!

After patching server my feature was gone....
This warning means:
“This template is not associated with any feature”

This point me to:
Install updated by BMIDE 11.3.0 feature once again.
This eliminated this yellow mark.

I now I can full update my data model by TEM.