Cancel
Showing results for 
Search instead for 
Did you mean: 

Dataset as Thumbnail

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

So we are using the AWC 3.2 and we do not want the default capability of Teamcenter of showing a dataset(jpg,png) as the thumbnail for an item.

 

I believe the below solution applies the fix for version 3.3.

https://docs.plm.automation.siemens.com/tdoc/aw/3.3/aw_html_collection/#uid:xid1350883

 

What would be your suggestions for version 3.2?

12 REPLIES

Re: Dataset as Thumbnail

Gears Phenom Gears Phenom
Gears Phenom

Did you try it on 3.2? I think it works the same just not documented until 3.3. 

 

Jamie

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Dataset as Thumbnail

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Yes, tried "If no thumbnail image is desired, remove all values from the TC__thumbnail_relation_order preference."

 but it did not work. The thumbnail is still shown.

https://docs.plm.automation.siemens.com/tdoc/tc/11.2/help/#uid:web_show_thumbnail_image

 

Hopefully this should fulfill the requirement.

Re: Dataset as Thumbnail

Gears Phenom Gears Phenom
Gears Phenom

What version of TC are you using? There are 2 preferences that work together and have been used since AW2.x. What are your values for both? 

TC__thumbnail_dataset_type_order

TC__thumbnail_relation_order

 

What is the behavior you want to see in AW -no thumbnail at all for anything? I know there are some issues with these preferences depending on your TC version and it is fix in specific versions. 

 

Jamie

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Dataset as Thumbnail

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

The default values are a list of relations used by our data model.

- IMAN Spec
- Reference

- etc

- etc

 

EDIT:EDIT TC 11.2.3

        : AWC 3.2

 

Re: Dataset as Thumbnail

Gears Phenom Gears Phenom
Gears Phenom

Similar problem reported against TC11.2.2.1 on PR#7854204 - says resolved in TC11.3. This says the preferences is not honoring the order. I would suspect that it also would not honor if you removed all values. You should call Gtac to confirm.

 

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Dataset as Thumbnail

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

WEB_show_thumbnail_image

 

DESCRIPTION

Determines whether to display thumbnail images in thin client pages.

 

This one also did not work.

 

And neither did removing all the values from -

TC__thumbnail_dataset_type_order

TC__thumbnail_relation_order

 

Is Calling GTAC the only option?

Re: Dataset as Thumbnail

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Jamie,

 

Can you please point me towards PR#7854204? How do I look into the problem details?

 

Thanks in advance!

Re: Dataset as Thumbnail

Gears Phenom Gears Phenom
Gears Phenom

Do you have a webkey account to log into the Gtac Solution Center site? You can search for similar problems that have been reported to Gtac. They will have IR, PR or ER number listed. If you search by your preferences, you can find the PR that I mentioned before.

 

https://solutions.industrysoftware.automation.siemens.com/

 

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Dataset as Thumbnail

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

 

I do have a WebKey login, however after logging in this is all I get. :(

EDIT: I login to WebKey, but I have never provided a SoldTo/Webkey Access Code. So I think I need to start there.

 

Page Forbidden

Access to the requested resource is forbidden.

 

Return to WebKey Login page