Cancel
Showing results for 
Search instead for 
Did you mean: 

Dataset created, application is not launched and 'open with' does not offer 'others'

Legend
Legend

Hello,

I have been following the documented steps at:

 

https://support.industrysoftware.automation.siemens.com/docs/teamcenter/10.1.3/help/#uid:index_plm00...

 

and after adding the type and the tool from BMIDE it has become available on Teamcenter. The new datasets can be imported but the associated application does not start when they are checked out. The path to the application has been added to system's path to ensure that it is found during runtime. The default viewer is opened instead. Any hint of what I am doing wrong? 

 

Also, no option for 'other' application under 'open with' menu item. The only available applications under the menu are those of Teamcenter.

 

Any idea of what logfile I should inspect to check where Teamcenter is failing to launch the external application?

 

Thank you.

1 REPLY 1

Re: Dataset created, application is not launched and 'open with' does not offer 'others'

Legend
Legend

My fault!

The file type was not associated at system level.