Cancel
Showing results for 
Search instead for 
Did you mean: 

Datasets inside the second ItemRevision do not get released status

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys, I hope you can help me with this.

I have an ItemRevision which has another ItemRevision inside (see the picture). When I run WF on the first ItemRevision the second ItemRevision also gets the release status (this is ok). But what I want is that also datasets inside this second Item revision get the status. One way is that I choose both ItemRevisions and run WF on them (this works). But my question is if it is possible that if I run WF on the first ItemRevision also children-datasets from the second one get the status. Currently in the WF I have set:

EPM-attach-related-object with IMAN_specification, IMAN_reference, PSBOMViewRevision.

Does anybody know if this is possible or only the option with both selected revision is the right one.

 

Thanks.

Janez

4 REPLIES

Re: Datasets inside the second ItemRevision do not get released status

Siemens Genius Siemens Genius
Siemens Genius

Hallo Janez,

 

Check the relation between the datasets & the Item Revision and include them in the "EPM-attach-related-objects" handler.

Use one handler per relation. Thanks

Re: Datasets inside the second ItemRevision do not get released status

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi ArunG,

I was also thinking like you have written. But the problem is that the 1'st ItemRev only has relation to second ItemRev and not its dataset (pictures attached), so I believe that is why it is not setting status to them. That is why my question is if it is possible to set the status to them.

Re: Datasets inside the second ItemRevision do not get released status

Siemens Genius Siemens Genius
Siemens Genius

OK. In that case i would use two Tasks.

 

First task defining:

EPM-attach-related-objects -relation = IMAN_reference -attachment=target

This would first attach your first revision to the workflow target.

 

On second Task:

EPM-attach-related-objects -relation = IMAN_specification -attachment=target

This should attach all the datasets to the workflow target.

 

Give it a try! Thanks

Re: Datasets inside the second ItemRevision do not get released status

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks a lot, this worked.

 

Regards

Janez