Cancel
Showing results for 
Search instead for 
Did you mean: 

Define a change the text displayed in the late notification message

Hi everyone,

I would like to know if there is any way to change the message that is displayed in the late notification message.

The screenshot of the current text is given, i would like to add the task and process name into that message.

Currently its unclear which task from which workflow process is overdue that sent the late notification.

Can we create a handler that would define the text as we do in the EPM-notify handler, wherein we can input the subject of the mail notification.

 

 

late notification.PNG

 

Thanks and regards,

Sanket Pusalkar

5 REPLIES

Re: Define a change the text displayed in the late notification message

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

 

 

I don't think there is a way to change the text.

You may want to reach out to GTAC. We did the same for this behavior.

 

Harish

Re: Define a change the text displayed in the late notification message

Hi harish,
Goin to GTAC will be the last resort.
Did GTAC provide you with the solution?
Do you have a different text here now?
Could you please share related documentation, if you have any?



Thanks and Regards,
Sanket Pusalkar.

Re: Define a change the text displayed in the late notification message

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
@Sanket, the question you should ask @harish is: What ER number did GTAC give you so that I can add our Company to the ER too? The more Companies linked to an ER the more likely Development will be tasked to look at it.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Define a change the text displayed in the late notification message

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Sanket,

 

don't think I have the ER number with me...it was for a customer few years back.

The way we had reported the issue to GTAC was lack of arguments in epm-late-notification handler to configure the notification message.

 

Harish

Re: Define a change the text displayed in the late notification message

Dear Harish,
I found quite a few PRs on GTAC stating similar problems, one of it said,
it was converted into an ER.
Others didnt have a response from GTAC side.



Thanks and Regards,
Sanket Pusalkar.