Cancel
Showing results for 
Search instead for 
Did you mean: 

Detect configurations of pre-installled Teamcenter

Builder
Builder

Hi all.

 

I want to know if there is a proper method to detect all the configurations of a pre installed Teamcenter like as port numbers of ServerManager, 4-Tier, Web-Tier, Dispatcher, Proxy, and so on?

 

Is it a command or any configuration file which includes such data at all?

 

Thanks

1 REPLY

Re: Detect configurations of pre-installled Teamcenter

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
TC_ROOT\install\configuration.xml will show how it was installed and modified through TEM. Manual edits are not tracked. You would need to review this file on each server where Tc is installed.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4