Cancel
Showing results for 
Search instead for 
Did you mean: 

Difference between the arguments of the EPM-notify-report handler

Phenom
Phenom

Good afternoon,
What is the difference between the arguments of the EPM-notify-report handler? According to the description, they are the same (or very similar):

h1.png

And very similar arguments:

h2.pngIn which cases should I use, without PROPOSED, and in which with PROPOSED?

3 REPLIES

Re: Difference between the arguments of the EPM-notify-report handler

Siemens Phenom Siemens Phenom
Siemens Phenom

I suspect this is a defect in the documentation for this handler.

Elsewhere in the doc you will see definitions similar to the following;

 

$REVIEWERS

    Builds a list of all users who are reviewers in the same task level as the current reviewer and sends e-mail to all of them.

$PROPOSED_REVIEWERS

    Sends e-mail to all members assigned as the proposed reviewers of the first target object in the workflow process.

$RESPONSIBLE_PARTY

    Sends e-mail to the designated responsible party for the task.

$PROPOSED_RESPONSIBLE_PARTY

    Sends e-mail to the member assigned as the proposed responsible party of the first target object in the workflow process.

 

 

PROPOSED_REVIEWERS and PROPOSED_RESPONSIBLE_PARTY are keywords that map to a dynamic participant on the workflow target.  You can see the definition of the participants in BMIDE.

RESPONSIBLE_PARTY is the current responsible party for the task.

REVIEWERS is derived from the signoffs for the task.

Re: Difference between the arguments of the EPM-notify-report handler

Phenom
Phenom

Good afternoon, thanks for the answer.
This is used only for the Change Management object? As far as I know, only these objects are assigned dynamic participants

Re: Difference between the arguments of the EPM-notify-report handler

Siemens Phenom Siemens Phenom
Siemens Phenom

It's possible to define your own dynamic participants in BMIDE and specify to which objects they apply (though it must be a subtype of ItemRevision).  When you define the participant type you can specify the keyword you wish to use in workflow handlers, and if it should be a single assignee, or multiple.

 

Having said that some of the handlers do have keywords that are documented as specific to change objects.