Cancel
Showing results for 
Search instead for 
Did you mean: 

Dispatcher - can't create task

Valued Contributor
Valued Contributor

Hi all,

 

I've been trying to get the dispatcher run on our test system.

tried to install all three components but were somewhat overwhelmed by the setup preferences neccecary to fill out.

Hope I did the setup correct, but it's likely I missed something.

 

We are working with a 4-tier TCRS 11.3 setup.

I modified the installation trough TEM to install Dispatcher.

 

There are two main issue right now:

  1. The RAC has a "Translation" menu, but is not showing the "Translate" button.
  2. When running "dispatcher_create_rqst trough" to run a basic "tozipfile" test with a WordX dataset CMD I get errors.

 

Other issue that seems like an indication of some configuration errors is that I can't shutdown the dispatcher client (both service and cmd). Shows an error and wont stop and/or start without a server reboot.

 

What i've done so far (after installing dispatcher):

  • Try using windows services
  • Try using CMD services
  • Changed logging to DEBUG, (to me no obvious clues)
  • Try creating a translate taks trough CMD
  • Added "tozipfile" service to ETS.TRANSLATORS.SIEMENS to make the translate service available in the RAC

 

I'm stuck and do'nt know what to look for right now.

Any suggestions?

 

Attached you'll find the log files and screenshots.

9 REPLIES 9

Re: Dispatcher - can't create task

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Problem1: To see the translation menu in RAC, install feature "Dispatcher Client for Rich Client" via TEM.

 

Problem 2: Make sure the access rule for your dispatcher user is created as mentioned in doc (see below)

 

 

After installation, you must add a rule to the access rule tree permitting the translation service proxy user to update attributes of a DispatcherRequest object. If this access rule is not created correctly, the dispatcher client reports errors.

  1. Log on to the Teamcenter rich client as a system administrator.

  2. Open Access Manager.

  3. In Access Manager, add the following rule to the rule tree under Has Class (POM_application_object)Working:

    • Condition =Has Class

    • Value =DispatcherRequest

    • ACL Name =DispatcherRequest

    • ACE Type of Accessor =User

    • ACE ID of Accessor =DC-Proxy-User-ID

    • ACE Privilege =Write

    • ACE Privilege Value =Grant

    • ACE Privilege =Delete

    • ACE Privilege Value =Grant

    Note

    This rule applies only to the standard Access Manager rule tree. If custom rules are specified for the installation, your custom rules must be modified to provide the equivalent access of this rule. The DC-Proxy-User must be the same user that was specified during installation using the Teamcenter Environment Manager installation tool.

Re: Dispatcher - can't create task

Valued Contributor
Valued Contributor

Thanks for the fast reply!

 

I have "Dispatcher Client for Rich Client" installed already.

 

Access rule was automatically created on install.

 

Do you have any other directions? 

Re: Dispatcher - can't create task

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Next step would be to create access rule for "Dataset" class, so that the Dispatcher User can create/edit the datasets.

Re: Dispatcher - can't create task

Valued Contributor
Valued Contributor
Sorry, can you be a bit more specific in what to add?
Do I add the new rule to the "Has Class (POM_application_object)→Working", next to the "Has Class (DispatcherRequest)→DispatcherRequest" or do I add the user to the ACL of the existing rule "Has Class (Dataset)→TcX"?

Re: Dispatcher - can't create task

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I added an ACL as shown in image under: Has Class (POM_application_object) -> Working

Re: Dispatcher - can't create task

Valued Contributor
Valued Contributor

Okey, finally got a chance to continue this implementation and added the ACL.

 

Started the CMD dispatcher services.

Retried starting translation trough CMD.

Result is a different error stating the dataset could not be found.

 

D:\PLM\TCRS112\tc_menu>DISPATCHER_create_rqst -i="1000051" -r="-" -dn="Translate
Test001" -dt="MS WordX" -dv=2 -pr=1 -pn="SIEMENS" -tn="tozipfile"
DISPATCHER_create_rqst ( May 15 2017 16:39:53 )
version number NOT specified, using latest
Could not find dataset <TranslateTest001>, version 2
Dispatcher create request FAILED ( -4 )

Searched for any info on error -4 but did not manage to find it.

 

Tried to not specify a dataset version but same error, got the current version form the dataset properties found in the RAC. Perhaps still a ACL problem?

Re: Dispatcher - can't create task

Siemens Phenom Siemens Phenom
Siemens Phenom

This may not be the problem, but you have a space in your -dt argument; "MS WordX".  While this is the display name of the dataset type its real name is "MSWordX".

Re: Dispatcher - can't create task

Valued Contributor
Valued Contributor

That did the trick!

 

Got a new zip dataset in the item revision containing the docx.

 

Will create a different thread to get the Translate button in RAC visible.

Re: Dispatcher - can't create task

Valued Contributor
Valued Contributor

To inform others, no need for new thread, found the solution here

 

It's a TC RapidStart installation, so the command is disabled by default.

To enable it in the RAC, open the "Command suppression" application:
2018-05-09 13_20_48-PDM-TEST01 (10 - 10.10.10.64 - Verbinding met extern bureaublad.png

 

After setting the "Translate..." command to "Show", it shows up:

2018-05-09 13_25_29-PDM-TEST01 (10 - 10.10.10.64 - Verbinding met extern bureaublad.png

And it works!