Cancel
Showing results for 
Search instead for 
Did you mean: 

Dispatcher in 4 Tier Environment

Creator
Creator

HI, Can we Use dispatcher client to connect from 4 Tier environment instead of configuring from 2t

is this possible?

 

Thanks

Kishore

4 REPLIES 4

Re: Dispatcher in 4 Tier Environment

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Unfortunately that is not supported yet.

 

Best Regards

Projyal

Re: Dispatcher in 4 Tier Environment

Creator
Creator

Thanks Projyal...

Re: Dispatcher in 4 Tier Environment

Genius
Genius

Hello Kishore,

 

I think you can create an OTW instance and add Dispatcher Client for Rich Client for Four Tier.

 

Hope this helps!

Cheers.

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Dispatcher in 4 Tier Environment

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Nope. The plugin for Rich Client (OTW or TEM) enables the dispatcher menu for administering jobs. It is not a Dispatcher Client.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4