Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Dispatcher not processing any requests

Phenom
Phenom

Dear all,

 

I have a successfully running dispatcher on TC9 and now I installed the same on TC11.2.1.

 

Scheduler, Module and DC are running successfully. DC and module are connected to Scheduler.

 

But I see following problems:

 

1. Though DC says it started successfully, there is no message about connecting to TcServer

2. All 3 components are running on CMD and show no response on creating a Translation request

3. AdminClient shows all Translation requests are stuck at INITIAL stage.

3. No task folders are created under StagingDirectory i.e. it's always empty.

4. 2099 port specified for DispClient is unused.

5. No error message is displayed

 

I compared and verified all settings with TC9 dispatcher and I don't see any difference.

 

Any idea what's wrong or how to troubleshoot this problem ?

 

Thanks in advance!

9 REPLIES 9

Re: Dispatcher not processing any requests

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
One of the challenges with Dispatcher is that you have to uninstall, usually before the upgrade, then reinstall after the upgrade. I've read an SFB (can't seem to find it now) about it and follow that procedure when upgrading. Try uninstall/reinstall.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Dispatcher not processing any requests

Siemens Phenom Siemens Phenom
Siemens Phenom

If all requests remain at INITIAL then the Dispatcher Client is not working.  Start there because the Scheduler and Modules are not getting the data they need from the Dispatcher Client.


 


 


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Dispatcher not processing any requests

Phenom
Phenom
Thanks Randy for the hint. I found the SFB and will try to follow the same.

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=dispatcherclient&dt=s...

Re: Dispatcher not processing any requests

Phenom
Phenom
Thanks Larry for the response. Yes that's where I'm going to start...

Re: Dispatcher not processing any requests

Phenom
Phenom

After updating the DC libs, I have been struggling with following error at updateTranslationRequest. Any idea ?

 

2017-03-17 11: 27: 17,517 INFO - Processing the database requests is started.
2017-03-17 11: 27: 17.517 TRACE - Extractor.start ()
2017-03-17 11: 27: 17,517 DEBUG - Database re-registration is planned. Interval in minutes: 1440
2017-03-17 11: 27: 17,518 TRACE - Creating MBeans ...
2017-03-17 11: 27: 17,591 TRACE - Done registering MBeans
2017-03-17 11: 27: 17,592 DBGHG - [queryRequests] Begin query ...
2017-03-17 11: 27: 17,893 DBGHG - Query found 21 requests.
2017-03-17 11: 27: 17,894 DBGHG - [updateTranslationRequest] Begin update requests ...
2017-03-17 11: 27: 19,104 DBGHG - [checkPartialErrrors] 1 errors were found.
2017-03-17 11: 27: 19.104 DBGHG - Error code is 515001
2017-03-17 11: 27: 19,105 ERROR - Access denied - please check the access rules according to the correct configuration or contact the administrator.
2017-03-17 11: 27: 19.105 INFO service stopped ...
2017-03-17 11: 27: 19.105 TRACE - logout begin ...
2017-03-17 11: 27: 19,106 TRACE - ConnectionManager.disconnect begins ...

2017-03-17 11:27:20,951 ERROR - Exception.
java.lang.Exception: Access denied - please check the access rules according to the correct configuration or contact the administrator.

    at com.teamcenter.ets.extract.Extractor.<init>(Extractor.java:272)
    at com.teamcenter.ets.ServiceMode.startService(ServiceMode.java:67)
    at com.teamcenter.ets.ServiceMode.main(ServiceMode.java:256)
Caused by: java.lang.Exception: Access denied - please check the access rules according to the correct configuration or contact the administrator.
    at com.teamcenter.ets.soa.TeamcenterServerProxy.checkPartialErrrors(TeamcenterServerProxy.java:1392)
    at com.teamcenter.ets.soa.TeamcenterServerProxy.updateTranslationRequest(TeamcenterServerProxy.java:529)
    at com.teamcenter.ets.request.TranslationRequest.updateState(TranslationRequest.java:460)
    at com.teamcenter.ets.request.TranslationRequest.updateTransRqstState(TranslationRequest.java:549)
    at com.teamcenter.ets.extract.Extractor.getNext(Extractor.java:763)
    at com.teamcenter.ets.extract.Extractor.start(Extractor.java:308)
    at com.teamcenter.ets.extract.Extractor.<init>(Extractor.java:266)
    ... 2 more

Re: Dispatcher not processing any requests

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

It looks like "dcproxy" doesn't have access rights to the objects.

DispatcherRequest ACL

Has Class(POM_application_object) ? Working

Condition

Has Class

Value

DispatcherRequest

ACL Name

DispatcherRequest

ACE Type of Accessor

User

ACE ID of Accessor

dcproxy

ACE Privilege

Write / Delete

ACE Privilege Value

Grant


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Dispatcher not processing any requests

Phenom
Phenom
Thanks Randy, this worked for me.

In Tc9, it worked without creating an ACL and I also checked and found that such an ACL does not exist.

I'm wondering what has changed in TC11. Any idea ?

Re: Dispatcher not processing any requests

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I've been adding the ACL since 2007 so I'm not sure why it worked in Tc9.1 without it. Maybe you used a different account in Tc9.1 to run translations instead of dcproxy?

Thank you, you were my 100th accepted solution and I earned the "Enlightened" badge.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Dispatcher not processing any requests

Phenom
Phenom
Congratulations and thank you for 'enlightening' us :)

Yes, I used a different account in TC9.1. But I also used the same account in TC11.2 as well.