Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Does the Workflow can Automatically Trigger Create Revision ?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

lets say i started workflow from item-00022/A than there is rejection from some action that automatically create item-00022/B, is it possible ?

1 REPLY 1

Re: Does the Workflow can Automatically Trigger Create Revision ?

Phenom
Phenom

I have seen this done with a custom handler, but not out of the box..Happy to be proven wrong though :-)

 

If you can't create your own handler, maybe an alternitive would be use PIE-export-to-plmxmlfile and then EPM-run-external-command which could call some custom code which manipulates the data in the xml file and then plmxml_import could create it?

 

Just an idea.

 

Richard Bennett

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk