Cancel
Showing results for 
Search instead for 
Did you mean: 

Double Item Revisions

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everybody,

 

By a customer, and only by a certain user we are seeing double Item Revisions.

 

Deleting one version of the two deletes them both.

 

In GTAC Solution Center is not easy to search for this incident since writing double or duplicated gives more than 700 results.

 

Logfiles aren't showing anything special...

I tried deleteing the RAC, it didn't help too...

 

Its Teamcenter 10, 4-Tier.

 

Thanks in Advance

 

Greetings from Germany

M

3 REPLIES 3

Re: Double Item Revisions

When you meant 2 revisions, you meant 2 sequence ?

whether revisions are displayed like <item_id>/<rev_id>;<sequence_num> ( 0001322/1;1,0001322/1;2 ) ?

Using Print object view, can you check whether UID for both the revs are same?

Re: Double Item Revisions

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you for your reply

 

Its is showing it like this:

 

000-000-001- Test Item

   000-000-001Bom View

   000-000-001/--

   000-000-001/B

   000-000-001/C

   000-000-001/D

   000-000-001/--

   000-000-001/B

   000-000-001/C

   000-000-001/D

 

The revisions are of the type: designelemetrevision. (They are created with Autodesk Inventor Proffesional 2015).

Its only one user who is seeing these double revisions. It doesn't matter if he is the owner or of the item or not...

When deleting one revision of the 2 the other one is deleted too.

 

Thanks in Advance

Greetings,

M

 

 

 

 

 

 

Re: Double Item Revisions

That is strange behavior.. Is this happening for only this type of item or for other item types as well ( OOTB object preferably)?

 

If this happening for only one user, then try these options:-

1. Login to TC Thinclient as that user and see whether it displays 2 revisions..

         If user is seeing 2 revisions in thin client as well, some user preference change might be reason.

         If user is seeing this behaviour only in RAC, then the problem might be in user's temp folder. Try clearing Siemens,Teamcenter,Temp folders