Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: E-mail Notification Problem

Siemens Genius Siemens Genius
Siemens Genius

Mmmm,

ok,

Please go to a workstation, and please to checked connecting between workstation and mail server,because each of "2 Tier RAC" it a separately Teamcenter Server:)

 

All the best, Alexey.

Re: E-mail Notification Problem

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You can look into hMailServer (open source) to send smtp for Teamcenter notifications that are not tied to your corporate mail system if that is your roadblock. Easy to configure and use.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: E-mail Notification Problem

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi All

 

 

Thank you for the help.

Well! I resolved the issue. 

 

The variable TC_TMP_DIR was not set for me. On setting it , it worked.

 

Cheers

Ambuj

Re: E-mail Notification Problem

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi @Ambuj ,

Thanks for information , Could you give me detail with that varaiable?

 

Best Regards

Gurkan

Re: E-mail Notification Problem

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@GurkanAlkan:

 

Let me know exactly what details are you looking for ?

The set up remains same as posted previously from your side. The same set up exist except the

server.

 

TC_TMP_DIR : It is the folder where the user must have the write access as all the content related to mail from the teamcenter comes at this folder.

 

Ambuj

                       

Re: E-mail Notification Problem

Siemens Genius Siemens Genius
Siemens Genius

For first, please make a folder on drive C (on Teamcenter server side) with name "Temp", if you will check TC parameter such as "Transient_Volume_RootDir" you will see that it has a value C:\Temp\blblblblblblblba (in most default cases)

The variable TC_TMP_DIR is initialized via tc_profilevars.bat and you don`t need to rewrite it

All the best, Alexey.

Re: E-mail Notification Problem

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi

 

Yes, TC_TMP_DIR  is present in the tc_profilevars.bat

However, it was commented out, so I set it as environment variable

 

Ambuj