Cancel
Showing results for 
Search instead for 
Did you mean: 

EIM_does_table_exist: POM_AUDITED_USERS is not there

Phenom
Phenom

I have configured Applet-Free-SSO with TC11.2.1, Tomcat & IIS 7.5.

 

SSO token is generated successfully, but TC-Session login fails. The syslog shows following error:

 

--------------------------------------------------------------------------------------------------------------------------------------------

EIM_does_table_exist:  POM_AUDITED_USERS is not there - Teamcenter.POM at D:\workdir\tc1121w1116_64\src\foundation\pom\eim\eim_tables.cxx(933)

ERROR 515240: ITK_init_module_login failed - Teamcenter.CoreModelGeneral.tc at D:\workdir\tc1121w1116_64\src\core\tc\infomanager_itk.cxx(2184)
ERROR - 2017/05/02-14:44:37.652 UTC - XPLM-GUL-NB.97342.01.Anonymous.00001.Mgr.Svr.UnknownClient.00001 - loginUser::initialise failed for 515007 - Teamcenter at D:\workdir\tc1121w1116_64\src\core\tc\loginuser.cxx(525)

--------------------------------------------------------------------------------------------------------------------------------------------

 

Any idea why is this error thrown ?

 

I also have attached the syslog.

 

Thanks in advance for your inputs!

4 REPLIES

Re: EIM_does_table_exist: POM_AUDITED_USERS is not there

Phenom
Phenom

Solved: As per this SFB, SSO login service war file and SSO identity service war must be deployed on different hosts.

 

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&file_type=html&q=TCSSO_...

Re: EIM_does_table_exist: POM_AUDITED_USERS is not there

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The SFB states that TcServer and the SSO Identity Service need to be on separate hosts. TcServer is either Pool Manager (J2EE) or Server Manager (.NET). I think the SSO login service war and SSO identity service war can be deployed on the same server as long as it doesn't also have TcServer running on it.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: EIM_does_table_exist: POM_AUDITED_USERS is not there

Phenom
Phenom
Hello Randy, yes you are right, it was my misreading.
And that makes it also more organised as web app server will run only on one host, unlike the current situation in my case.
Thanks for pointing it out!

Re: EIM_does_table_exist: POM_AUDITED_USERS is not there

Phenom
Phenom

Also the SFB nowhere mentions the EIM_does_table_exist, like I posted above.

 

After I enabled journaling and tracebacks for teamcenter logging, I got below error in syslog. This error lead me to the SFB.

 

TCSSO login failed for user [infodba]. Error type [TCSSO_SSOSystemException]
 text [General HTTP exception]