Cancel
Showing results for 
Search instead for 
Did you mean: 

Error Code 108 after Live Update hot Deploy

Experimenter
Experimenter

Hello everyone, 

 

I got the following message after deploying a live update where we wanted to add a supplier to our TC LOV.   I've checked if error message class, and tried to do what it recommends to do, but we haven't been able to find a solution. 

 

*************************************************************************
**************************** INSTALL BEGINS *****************************
*************************************************************************
*************************************************************************
Time of Install: Wed Jun 13 15:55:31 CEST 2018
Operating System: Windows Server 2012
OS Version: 6.2
OS Arch: amd64
User Name: teamcenterservice
User Home: C:\Users\teamcenterservice
Application: tceng
Application Version:10000.1.0.30
Java Runtime Version: 1.7.0_45-b18
Java Installation Directory: E:\SIEMENS\JRE17u45\x64

Current Directory: E:\SIEMENS\TC101\install

Launched from media? false
Launched from RTM? false
Launched from patch? false
Launched from minikit? false
*************************************************************************
*************************************************************************
No debugging options are enabled
*************************************************************************
*************************************************************************
No defaults files are in use
*************************************************************************
*************************************************************************
The following Teamcenter-related environment variables were set when TEM was launched
PATH =
C:\Windows\system32
C:\Windows
C:\Windows\System32\Wbem
C:\Windows\System32\WindowsPowerShell\v1.0\
PATHEXT = ".COM;.EXE;.BAT;.CMD;.VBS;.VBE;.JS;.JSE;.WSF;.WSH;.MSC"
SPLM_LICENSE_SERVER = "28000@NWS4008.STADLERRAIL.CH"
TC_JRE_HOME = "E:\SIEMENS\JRE17u45\x64"
TC_TMP_DIR = "F:\SIEMENS\TC_TMP"
TEMP = "C:\Users\TEAMCE~1\AppData\Local\Temp\2"
TEM_JRE = "E:\SIEMENS\JRE17u45\x64"
TEM_SPLASH = "-splash:./install/Splash.jpg"
TMP = "C:\Users\TEAMCE~1\AppData\Local\Temp\2"
UGII_BASE_DIR = "E:\SIEMENS\NX10"
UGII_FLEX_NOTE = "ON"
UGII_LANG = "spanish"
UGII_ROOT_DIR = "E:\SIEMENS\NX10\UGII\"
UGII_TMP_DIR = "E:\tmp\NX10"
*************************************************************************
*************************************************************************
Gopher Information
RTM : Z:\TC10.1\Tc10.1.0\Tc10.1.0_win64

Core paths
Z:\TC10.1\Tc10.1.0\Tc10.1.0_win64
Z:\TC10.1\Tc10.1.1.1\wntx64
Z:\TC10.1\Tc10.1.3\wntx64\wntx64
Browsed paths
\\nws4100\software$\NX\TC10.1\Config_Model_Changes_10.1\02 BMIDE\Productivo\Live Update\2018_06_13_15-51-42
*************************************************************************
*************************************************************************
Patching Information
201404101855: Z:\TC10.1\Tc10.1.1.1\wntx64
201504101756: Z:\TC10.1\Tc10.1.3\wntx64\wntx64
*************************************************************************
*************************************************************************
Operation: Install Mode
Config ID: TCVV
Recovery Mode? false
Maintenance Mode? true

Features currently installed
VC 2005/2008/2010 Redistributables
FMS Server Cache
Teamcenter Foundation
NX Integration
Java EE Based Server Manager
Action Manager Service
Subscription Manager Service
Task Manager Service
Client Communication System
2-tier server configurations
JtUtilities Support
Teamcenter Rich Client 2-tier
Translation Service Database Module/Data Model
Integration for CATIA/Integration for CATIA
Vossloh custom template/Data Model
Teamcenter Integration for NX/Data Model
Teamcenter Integration for NX/Runtime Server
NX Manager for Rich Client
Dispatcher Client
Change Management/Data Model
Features to be added
None
Features to be removed
None
Features to be deprecated
None
*************************************************************************
Loading E:\SIEMENS\TC101\install\uninstall.xml
=====================================================
Processing <maintenance> feature Teamcenter Foundation
Time: Wed Jun 13 15:55:31 CEST 2018
=====================================================
*** Processing block Teamcenter Foundation/maintenance:0
Running com.teamcenter.install.tceng.base.DatabaseSteps
***
*** Running com.teamcenter.install.tceng.base.DatabaseSteps
***
Updating database
Setting up Teamcenter shell

Executing [set IMAN_ROOT=E:\SIEMENS\TC101]

Executing [set IMAN_DATA=E:\PLM_DATA\TCDATAS\TC101\TCVV]

Executing [set TC_ROOT=E:\SIEMENS\TC101]

Executing [set TC_DATA=E:\PLM_DATA\TCDATAS\TC101\TCVV]

Executing ["E:\PLM_DATA\TCDATAS\TC101\TCVV\tc_profilevars"]
Output from command: "E:\PLM_DATA\TCDATAS\TC101\TCVV\tc_profilevars"
command_exit=0
Exit Status 0, elapsed time 0:00:00

Executing [set TNS_ADMIN=E:\PLM_DATA\TCDATAS\TC101\TCVV]

Executing [set IMAN_BYPASS_CANNED_METHODS=ALL]

Executing [set BYPASS_RULES=ON]

Executing [set NR_BYPASS=ON]

Executing [set BMF_BYPASS_ALL_EXTENSION_RULES=ON]

Executing [set TC_USE_METADATA_SHARED_MEMORY=FALSE]

Executing [set INSTALL_IN_PROGRESS_MODE=true]

Executing [set TC_KEEP_SYSTEM_LOG=true]

Executing [set IMAN_KEEP_SYSTEM_LOG=true]

Executing [set IMAN_TMP_DIR=E:\SIEMENS\TC101\logs\1806131555]

Executing [set TC_TMP_DIR=E:\SIEMENS\TC101\logs\1806131555]

Executing [set LANGID=EN]

Executing [cd /D "E:\SIEMENS\TC101\logs"]
Output from command: cd /D "E:\SIEMENS\TC101\logs"
command_exit=0
Exit Status 0, elapsed time 0:00:00
...Done
Updating database: ops data deploy

Executing ["E:\SIEMENS\TC101\bin\bmide_deployment_lock.exe" -u=infodba -p=Inf0dba_tcvv -g=dba -lock]
Output from command: "E:\SIEMENS\TC101\bin\bmide_deployment_lock.exe" -u=infodba -p=Inf0dba_tcvv -g=dba -lock

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

***** BMIDE deployment lock utility results *****

Process lock operation

Success

***** BMIDE deployment lock utility results *****
command_exit=0
Exit Status 0, elapsed time 0:00:03

Executing ["E:\SIEMENS\TC101\bin\manage_model_files.exe" -u=infodba -p=***** -g=dba -force=model -option=download]
Output from command: "E:\SIEMENS\TC101\bin\manage_model_files.exe" -u=infodba -p=***** -g=dba -force=model -option=download

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*
Downloading File: model.xml
Downloading File: model_lang.xml
command_exit=0
Exit Status 0, elapsed time 0:00:03

Executing [echo n | "E:\SIEMENS\TC101\install\install\unzip" -o -d"E:\SIEMENS\TC101" "\\nws4100\software$\NX\TC10.1\Config_Model_Changes_10.1\02 BMIDE\Productivo\Live Update\2018_06_13_15-51-42\vossloh_template_live_update.zip"]
...17 files
Copying file E:\SIEMENS\TC101\install\vossloh\client_vossloh.properties to E:\PLM_DATA\TCDATAS\TC101\TCVV\model\client_vossloh.properties
Deploying vossloh to TC_DATA
Copying file E:\SIEMENS\TC101\install\vossloh\vossloh_template.xml to E:\PLM_DATA\TCDATAS\TC101\TCVV\model\vossloh_template.xml
Copying file E:\SIEMENS\TC101\install\vossloh\vossloh_dependency.xml to E:\PLM_DATA\TCDATAS\TC101\TCVV\model\vossloh_dependency.xml
Copying directory E:\SIEMENS\TC101\install\vossloh\lang to E:\PLM_DATA\TCDATAS\TC101\TCVV\model\lang
Copying file E:\SIEMENS\TC101\install\vossloh\vossloh_icons.zip to E:\PLM_DATA\TCDATAS\TC101\TCVV\model\icons\vossloh_icons.zip

Executing ["E:\SIEMENS\TC101\bin\update_runner.bat" -u=infodba -p=***** -g=dba -templates=vossloh -isLiveUpdate=true -log=E:\SIEMENS\TC101\logs\update_runner.log]
Output from command: "E:\SIEMENS\TC101\bin\update_runner.bat" -u=infodba -p=***** -g=dba -templates=vossloh -isLiveUpdate=true -log=E:\SIEMENS\TC101\logs\update_runner.log
----------------------------------------------------------------------------
Update Templates to Teamcenter Database
Date: Wed Jun 13 03:55:38 PM 2018
----------------------------------------------------------------------------

 

Update start time: Wed Jun 13 03:55:38 PM 2018
Validating Teamcenter Environment for install...
Validating the Install script path for each template...
The following templates are going to be updated
vossloh
Install script for vossloh is E:\SIEMENS\TC101\install\vossloh\install_vossloh.default
Started the Update.
Restart index 0


----------------------------------------------------------------------------
Executing command 1 of 5...
Section: extractor
File: update_runner
Command: E:\SIEMENS\TC101\bin\business_model_extractor -u=infodba -p=***** -g=dba -outfile="E:\PLM_DATA\TCDATAS\TC101\TCVV\model\model.xml"
----------------------------------------------------------------------------
Command start time: Wed Jun 13 03:55:38 PM 2018
Output:

 

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

Extracting....

Extraction Completed.

Extracting Localizations....

Localization Extraction Completed.

Please refer [E:\SIEMENS\TC101\logs\1806131555\business_model_extractor_2018_06_13_15-55-41.log] for log information
Command end time: Wed Jun 13 03:57:16 PM 2018
Command duration: 1 minutes 37.430 seconds
Execution of command 1 is successful


----------------------------------------------------------------------------
Executing command 2 of 5...
Section: process-templates
File: update_runner
Command: bmide_processtemplates -u=infodba -p=***** -g=dba -mode=server -dir=E:\PLM_DATA\TCDATAS\TC101\TCVV\model -templates="vossloh" -deployvalidation=yes -addedtemplates="" -update=opsdata
----------------------------------------------------------------------------
Command start time: Wed Jun 13 03:57:16 PM 2018
Output:


Validating for deployment
Fetching BMIDE_ALLOW_LIVE_UPDATES preference

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

Exporting the following preferences to the file 'E:\PLM_DATA\TCDATAS\TC101\TCVV\model\live_update_preference.xml'...

BMIDE_ALLOW_LIVE_UPDATES
Done.

The report file is located at "E:\SIEMENS\TC101\logs\1806131555\preferences_manager_2018613155716.log".
Fetching deployment information for the installed templates

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

A report has been generated in the file E:\PLM_DATA\TCDATAS\TC101\TCVV\model\installed_templates_info.txt.
Fetching site information

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

File siteinfo.properties is created in the path E:\PLM_DATA\TCDATAS\TC101\TCVV\model
Getting deployment information for the template: vossloh
Adding Template to Master File...
Backing up the Consolidated Model File...
Backing up the Consolidated Model Localization File...
Finding Applicable Locales...
Finding Applicable Locales...
Creating the Consolidated Model File...
Creating the Localization Consolidated Model File...
Fetching Live Update preference

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

Exporting the following preferences to the file 'E:\PLM_DATA\TCDATAS\TC101\TCVV\model\live_update_preference.xml'...

Live Update
Done.

The report file is located at "E:\SIEMENS\TC101\logs\1806131555\preferences_manager_2018613155729.log".
Loading the Backup File...
Loading the Consolidated File...
Comparing the two Files...
Error while validating the delta for Live Update elements

***ERROR : This deploy has detected changes to data model elements that are blocked
by the administrator of the database. The entire deploy has been canceled.

To be able to deploy, you must do one of the following:
1. Request that the administrator enable the blocked elements listed below via the "Live Update" preference in RAC.
Once the administrator enables them, deploy again.
2. Back out the changes to the blocked elements listed below from your template and deploy again.
3. Create the blocked elements listed below in a standard BMIDE template project and perform a deployment using TEM.
This requires system down time.

----------------------------------------------------------------------------------------------------
Status |ElementType |Element XML Type |Element Name
----------------------------------------------------------------------------------------------------
Blocked |Class |TcClass |Fnd0VariantCritValidatn
Blocked |Class |TcClass |Fnd0VariantCriteriaExpr

**The backup of all files used for delta generation is available in E:\SIEMENS\TC101\logs\1806131555\compare_history\update\model_compare_2018_06_13_15-59-12.zip
Restoring the files from the database.
Updating FileVersions.txt before restoring files

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*
Downloading File: master.xml
Downloading File: vossloh_dependency.xml
Downloading File: vossloh_template.xml
Downloading File: vossloh_template_cs_CZ.xml
Downloading File: vossloh_template_de_DE.xml
Downloading File: vossloh_template_en_US.xml
Downloading File: vossloh_template_es_ES.xml
Downloading File: vossloh_template_fr_FR.xml
Downloading File: vossloh_template_it_IT.xml
Downloading File: vossloh_template_ja_JP.xml
Downloading File: vossloh_template_ko_KR.xml
Downloading File: vossloh_template_ru_RU.xml
Downloading File: vossloh_template_zh_CN.xml
Downloading File: vossloh_template_zh_TW.xml
java.lang.Exception
at com.teamcenter.bmide.foundation.core.consolidator.ProcessTemplates.generateDelta(Unknown Source)
at com.teamcenter.bmide.foundation.core.consolidator.ProcessTemplates.compareModels(Unknown Source)
at com.teamcenter.bmide.foundation.core.consolidator.ProcessTemplates.bmideDbSetup(Unknown Source)
at com.teamcenter.bmide.foundation.core.internal.consolidator.ProcessTemplatesMain.execute(Unknown Source)
at com.teamcenter.bmide.foundation.core.internal.consolidator.ProcessTemplatesMain.main(Unknown Source)
Done
Command end time: Wed Jun 13 03:59:15 PM 2018
Command duration: 1 minutes 59.924 seconds
ERROR: Execution of command 2 failed with error code 108
THE FAILED SECTION NAME : process-templates

Update end time: Wed Jun 13 03:59:15 PM 2018
Update duration: 3 minutes 37.365 seconds
Script execution failed.
UpdateRunner log file is created at: "E:\SIEMENS\TC101\logs\update_runner.log"
command_exit=-1
Exit Status -1, elapsed time 0:03:38

Executing ["E:\SIEMENS\TC101\bin\bmide_deployment_lock.exe" -u=infodba -p=Inf0dba_tcvv -g=dba -release]
Output from command: "E:\SIEMENS\TC101\bin\bmide_deployment_lock.exe" -u=infodba -p=Inf0dba_tcvv -g=dba -release

*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

***** BMIDE deployment lock utility results *****

Process release operation

Success

***** BMIDE deployment lock utility results *****
command_exit=0
Exit Status 0, elapsed time 0:00:02
An error occurred during execution. Stack trace follows...
com.teamcenter.install.tceng.base.DatabaseSteps.runUpdateRunner(DatabaseSteps.java:2874)
com.teamcenter.install.tceng.base.DatabaseSteps.updateDatabaseOpsData(DatabaseSteps.java:2820)
com.teamcenter.install.tceng.base.DatabaseSteps.updateDatabase(DatabaseSteps.java:2703)
sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
java.lang.reflect.Method.invoke(Unknown Source)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:209)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:115)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1342)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1280)
com.teamcenter.install.tem.struct.TcFeature.maintenance(TcFeature.java:1036)
com.teamcenter.install.tem.director.actions.MaintenanceAction.execute(MaintenanceAction.java:30)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:120)
com.teamcenter.install.tem.director.Director.run(Director.java:120)
java.lang.Thread.run(Unknown Source)
***
*** CANCELLED
***
=====================================================
Installation interrupted due the following reason:

Processing <maintenance> of feature Teamcenter Foundation failed: The update_runner utility failed with a return status of -1
Time: Wed Jun 13 15:59:35 CEST 2018
=====================================================
=====================================================
Begin Task: Log auto-archive creation
Time: Wed Jun 13 15:59:35 CEST 2018
=====================================================
Setting up Teamcenter shell

Executing [set IMAN_ROOT=E:\SIEMENS\TC101]

Executing [set IMAN_DATA=E:\PLM_DATA\TCDATAS\TC101\TCVV]

Executing [set TC_ROOT=E:\SIEMENS\TC101]

Executing [set TC_DATA=E:\PLM_DATA\TCDATAS\TC101\TCVV]

Executing ["E:\PLM_DATA\TCDATAS\TC101\TCVV\tc_profilevars"]
Output from command: "E:\PLM_DATA\TCDATAS\TC101\TCVV\tc_profilevars"
command_exit=0
Exit Status 0, elapsed time 0:00:00

Executing [set TNS_ADMIN=E:\PLM_DATA\TCDATAS\TC101\TCVV]

Executing [set IMAN_BYPASS_CANNED_METHODS=ALL]

Executing [set BYPASS_RULES=ON]

Executing [set NR_BYPASS=ON]

Executing [set BMF_BYPASS_ALL_EXTENSION_RULES=ON]

Executing [set TC_USE_METADATA_SHARED_MEMORY=FALSE]

Executing [set INSTALL_IN_PROGRESS_MODE=true]

Executing [set TC_KEEP_SYSTEM_LOG=true]

Executing [set IMAN_KEEP_SYSTEM_LOG=true]

Executing [set IMAN_TMP_DIR=E:\SIEMENS\TC101\logs\1806131555]

Executing [set TC_TMP_DIR=E:\SIEMENS\TC101\logs\1806131555]

Executing [set LANGID=EN]

Executing [cd /D "E:\SIEMENS\TC101\logs"]
Output from command: cd /D "E:\SIEMENS\TC101\logs"
command_exit=0
Exit Status 0, elapsed time 0:00:00
...Done

Executing [echo %TC_SSO_APP_ID%]
Creating log auto-arche

Executing ["E:\SIEMENS\TC101\bin\deploy_archive" -u=infodba -p=***** -g=dba -action=deploy -deploySource=tem -dir=E:\SIEMENS\TC101\logs\1806131555]
Output from command: "E:\SIEMENS\TC101\bin\deploy_archive" -u=infodba -p=***** -g=dba -action=deploy -deploySource=tem -dir=E:\SIEMENS\TC101\logs\1806131555

***** The deploy_archive utility STARTED! *****


-log=(null)


-action=deploy


-deploySource=tem


-dir=E:\SIEMENS\TC101\logs\1806131555


*
*
**** Library: seqlib - Version 1.0 (Compiled Apr 3 2014 08:40:05) ****
*
*

***** The deploy_archive utility completed SUCCESSFULLY! *****

command_exit=0
Exit Status 0, elapsed time 0:00:03
Auto-archive successfully created
=====================================================
Task completed successfully
Time: Wed Jun 13 15:59:39 CEST 2018
=====================================================

=====================================================
CommentStore
=====================================================
An internal error occured which has caused processing to stop.
Severity: 1 (Severe)

A log of the install can be found in {0}
Severity: 3 (Information)

=====================================================
Copying file E:\SIEMENS\TC101\install\configuration.xml to E:\SIEMENS\TC101\install\configuration1806131559.xml

1 REPLY 1

Re: Error Code 108 after Live Update hot Deploy

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
There is additional logs in E:\SIEMENS\TC101\logs\1806131555, especially for update_runner, that will likely give you a better indication of what is causing the error.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4