Cancel
Showing results for 
Search instead for 
Did you mean: 

Error Message "The requested SOA object is not loaded"

Experimenter
Experimenter

Hello Community,

 

i have a really big problem with Teamcenter / Siemens NX 10. I hope this is the place for my Problem.

 

Problem:

If I want to open an assembly from Teamcenter and in NX itself, I will get the Error Message:

 

"The requested SOA object property is not loaded"

 

Parts are no propblem just assemblies.

 

See attached the error message and also the log in file.

 

Maybe you can help me with my problem!

 

Thanks in advance!

 

Regards

4 REPLIES 4

Re: Error Message "The requested SOA object is not loaded"

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

You must add property 'bl_item' under Object "BOMLine" in one of the files (most probably the last one, adding it in all the files should not be an issue):
NxManagerMinimum
NxManagerDefault
NxManagerBrowse
NxManagerBlank

The files should be at %TC_DATA%\soa\policies

Re: Error Message "The requested SOA object is not loaded"

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, I think you should try to do what @Amol_XPLM wrote.
Do you have this problem on one computer or on multiple computers?

Re: Error Message "The requested SOA object is not loaded"

Experimenter
Experimenter

Thanks @Amol_XPLM for your fast response! I'am gonna try it today. I will let you know if it works.

 

@ArthurRMWe have the problem just on my computer in the network.

 

Thanks a lot for your support and fast help!

Re: Error Message "The requested SOA object is not loaded"

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, if this does not help, you can also try deleting the client cache in your user’s folder (delete Teamcenter and FCCCache folders)

 

Also on the Teamcenter server, delete and generate the client cache:

generate_client_meta_cache -u = infodba -p = infodba -g = dba -t delete all

generate_client_meta_cache -u = infodba -p = infodba -g = dba -t generate all