Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Error license NX integration

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

 

I have an issue with my NX integrated with Teamcenter.

When I lauch the "start_nxmanager.bat" i received this error:

Error NX integration.png

 

Here the features I have :

# NX11100             1 NX Mach 1 Design         

# NX13300             4 NX Mach 3 Ind Design     

# NX30120             7 NX Viewer                

# NX30122             1 NX Weld Assistant        

# SC12510             1 Simcenter Desktop Ad     

# SC13500             2 Simcenter Structures     

# SC30530             1 Simcenter Durability     

# TCADMIN             2 Teamcenter Admin  

 

My teamcenter is working well

My NX without Teamcenter is working well.

Do you have any idea to make my NX integration work ? Maybe an environment variable ?

 

Best regards.

15 REPLIES 15

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You need the nx_integration license. I don't know the number.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error license NX integration

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Randy,

 

Yes I Have that one, for example:

# NX11110            12 NX Mach 1 Design
#                                                12 assemblies
#                                                12 drafting
#                                                12 dxf_to_ug
#                                                12 dxfdwg
#                                                12 features_modeling
#                                                12 gateway
#                                                12 grip_execute
#                                                12 ideas_integration
#                                                12 iges
#                                                12 nx_freeform_1
#                                                12 nx_integration
#                                                12 nx_nas_bn_basic_dsk
#                                                12 nx_nastran_export
#                                                12 nx_sheet_metal
#                                                12 nx_spsd_stress
#                                                12 nx_spsd_vibration
#                                                12 pcf_package_file
#                                                12 pstudio_cons
#                                                12 pv_ugdatagenerator
#                                                12 sla_3d_systems
#                                                12 solid_modeling
#                                                12 step_ap203
#                                                12 step_ap214
#                                                12 teamcenter_designer
#                                                12 ug_kf_checker
#                                                12 ug_kf_execute
#                                                12 ug_nas_des
#                                                12 ug_smart_models
#                                                12 ug_to_dxf
#                                                12 ug_web_express
#                                                12 ugopen_menuscript
#                                                12 visview_base

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Are you launching via Teamcenter or trying to launch the script directly? Directly is bad. You have to launch Tc then launch NX from the button in Tc. Clicking the button calls the script for you. Be careful with multiple installations on the same client since the location of "start_nxmanager.bat" is stored in the registry. To launch NX manager w/o Tc you call ugraf as normal but with the -pim=yes argument.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error license NX integration

Genius
Genius

Make sure use the right license file

Re: Error license NX integration

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

- We have the same erro message from TC or from the script directly.

 

- We have 2 licenses Servers, 1 for TC ans 1 for NX.

The integration license are in the NX file.

 

How can we know if it reads on the right file ?

 

Best regards.

 

 

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Teamcenter and NX have to exist in the same license file. If you want them separate then you have to purchase an additional license (TC30600).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error license NX integration

Genius
Genius

try let the NX applications use the TC license server

Re: Error license NX integration

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Thank you.

 

Jason 27 :

How to let the NX applications use the TC license server ?

In the TC licence server we do not have NX licence.

 

Randy :

How can I merge the licences ?

 

Best regards.

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Merging the licenses requires that you coordinate with your CSR. The other option is to have your CSR add TC30600 to your Teamcenter license file:

The NX Integration with Teamcenter delivered with NX Mach products are packaged to work in an environment where the Teamcenter and NX license servers are on the same machine.
 
If a customer intends to work with a centralized Teamcenter license server and local NX license servers they must purchase the NX Embedded client (TC30600) for the centralized Teamcenter license server.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4