Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You can try this but I recommend to try combining through CSR first...
http://www.cecalc.ula.ve/documentacion/tutoriales/PGICDK/doc/flexuser/chap3.htm
(See 3.1.3 - Using Separate License Files on the Same Server Node)

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error license NX integration

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Randy,

 

Is it possible to have 2 files with 2 services in the same lmtools ?

To avoid merging the 2 files.

 

Regards.

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You can have two files with two services using the same lmtools but you cannot have to of the same services (uglmd) running on the same server. Even if you could it wouldn't solve your problem since you need the NX license to exist in the same license as Teamcenter or you need TC30600 to allow them to be separate. This isn't something you can defeat and maintain compliance.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error license NX integration

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

OK Randy.

 

Thank you very much, I will ask to our CSR to merge files.

 

Regards,

Re: Error license NX integration

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello Randy,

 

Is it possible to run two license files under one server node, if:

  • the files have different Sold-To,
  • the first file is for NX 12 and the second is for NX 11?

I tried to merge the text files under one server line, but it didn't work.

 

Regards,
Lidia

Re: Error license NX integration

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Merging the two files should work as long as the license software will run the latest. Unless these are node-locked (don't contain a SERVER line).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4