Cancel
Showing results for 
Search instead for 
Did you mean: 

Error while Patching TC 11.2.0 TO TC 11.2.3

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I tried to patch TC 11.2.0 to TC 11.2.3 and have this error below, any idea on this error ?

thanks.

 

 

 

image.pngimage.png

 

 

1 REPLY 1

Re: Error while Patching TC 11.2.0 TO TC 11.2.3

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
It can be many things but likely is the database compatibility setting:
- Open the MS SQL Server Management Studio
- Select that database that is being used for Teamcenter
- Right-Click on the Teamcenter database and select Properties
- In the Database Properties window/Select a page, click on options
- The current compatibility will be listed in the Compatibility level box.
- Change this to be the MS SQL 2012 server to match the version that this database is now being run on.
- Restart or refresh that database instance and then restart the Teamcenter upgrade.

The database calls have added the "TRY_CONVERT" command which is not available in earlier versions of the database:
MS SQL Version - Compatibility Level
2008 - 100
2012 - 110
2014 - 120
(you can Google it) If you are running 2012 then set the comp lvl to 110.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4