Cancel
Showing results for 
Search instead for 
Did you mean: 

Error while Patching TC 11.2.2 TO TC 11.2.3

Pioneer
Pioneer

I tried to patch TC 11.2.2 TO TC 11.2.3 and have this error below, any idea on this error ? thanks.

 

An error has occurred during the operation. Review the problem description and suggested actions. If a failure requires some input, the fields will be displayed below. Click the following log file to some technical information which may be useful in troubleshooting the issue.
NoSuchMethodException
Description
com.teamcenter.install.tceng.base.DatabaseSteps.revisioningCheck()

 

Note: Database is up and its located on the same sever as Foundation..

Please see attached file...

8 REPLIES

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

Log file will have more information.. Can you provide that?

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

Pioneer
Pioneer
i attached it on the part that has an error start..thanks for your concern..

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

Did you upgrade TEM before upgrating the TC ?

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

Pioneer
Pioneer
Nope, I just install directly the patch without upgrading TEM..do i need to upgrade TEM first ? if yes, any idea how to upgrade TEM ?

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

Genius
Genius

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

TEM upgrade might not be problem. But, since its looking for some class definition, possiblity that you didnt copy required files before starting patch process.

 

Also, try to start TEM as adminsitratior and start patch. 

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

I'm getting the same issue while patching, please let me know how you managed to resolve it..

 

"com.teamcenter.install.tceng.base.DatabaseSteps.revisioningCheck()"

Re: Error while Patching TC 11.2.2 TO TC 11.2.3

Valued Contributor
Valued Contributor
Download two zip files
TC 11.2.3 install.zip
TC 11.2.3 patch.zip

Unzip and Copy the TC 11.2.3 install folder into TC 11.2.2 install folder
Stop the TC services
Run the TEM in TC 11.2.2 to install the patch