Cancel
Showing results for 
Search instead for 
Did you mean: 

Error while adding SEEC feature

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

I want to install SEEC in Teamcenter 11.2 for Solid Edge 2019.

I lauched tem.bat from \TCRoot\install\tem.bat and I added the file feacture_seec.xml but when I started installtion

I get this error :

 

Description
The following command returned a value of 1
"install_runner.bat" -u=infodba -p=***** -g=dba -templates=seec

 

 

By the way I installed SEEC before in Teamcenter but after that Teamcenter stop working so I unistalled SEEC and Teamcenter and repeated everything.

 

 

Please help me to solve this problem.

Kind regards

15 REPLIES 15

Re: Error while adding SEEC feature

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, according to the integration matrix, Solid Edge 2019 supports integration with Teamcenter 11.3+

 

More details here, see the Integrations tab in the table:

 

Additional Resources -> Integrations Matrix

 

https://www.plm.automation.siemens.com/global/en/support/certifications.html

 

 

 

 

Re: Error while adding SEEC feature

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@ArthurRM thank you for your reply but according to the SEEC Admin Guide TC11.2 is supported by SE 2019:

 

TC & SE.PNG

 

When I download the package of SEEC, there is tc112 !!

seec.PNG

Re: Error while adding SEEC feature

Gears Phenom Gears Phenom
Gears Phenom

@Manel_PLM24  - you picture clearly shows it is supported at 11.2.2+ and not 11.2 because it isn't included in the box with the other version of 11.2.x. I also looked up the SFB to verify. Are you using just TC11.2 without any patch? If you are going to patch up TC, do that first and then add the SEEC template.

 

mp3.PNG

Jamie Griffis | PLM Solution Architect | Engineering USA

Re: Error while adding SEEC feature

Gears Phenom Gears Phenom
Gears Phenom

I would like to ask @Jamie_Griffis to help comment on your question, I unfortunately do not have access to Solid Edge

Re: Error while adding SEEC feature

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@Jamie_Griffis  and @ArthurRM  thank you both, so the easy solution is to work with SE 10. I find any change in TC very hard and there are always problems

Re: Error while adding SEEC feature

Gears Phenom Gears Phenom
Gears Phenom

@Manel_PLM24  - just keep in mind that ST10 hit End of Maintenance on Oct 31, 2018. I know TC can be a bit tricky, but you don't want to get too far outside of the maintenance window. I did that once and it was a much harder jump than what I had thought it would be to get to a supported version with both SE & TC involved. 

Jamie Griffis | PLM Solution Architect | Engineering USA

Re: Error while adding SEEC feature

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@Jamie_Griffis  thank you very much for this information I didn't know that before!

Re: Error while adding SEEC feature

Gears Phenom Gears Phenom
Gears Phenom

@Manel_PLM24 - keep track of SFB-SOLID_EDGE-8000986. They will updated it periodically with the latest info. You can always just search solution center for "Solid Edge EOM" to find the latest info.

 

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=SOlid+Edge+2019+matri...

Jamie Griffis | PLM Solution Architect | Engineering USA

Re: Error while adding SEEC feature

Gears Phenom Gears Phenom
Gears Phenom

Hmm, I'm a little surprised why Info from SFB <> Info from Integrations Matrix
TC 11.3+ <> TC 11.2.2