Cancel
Showing results for 
Search instead for 
Did you mean: 

Error while updating FMS master by tem.bat

Hi buddies,

 

I am getting some error while I am trying to update FMS master by environment manager...I have attached the snap...please reply me with a solution

6 REPLIES

Re: Error while updating FMS master by tem.bat

Phenom
Phenom

Could be due to write access problems. Please check that, also try running tem.bat as administrator.

If not, would be good to see some more details from log.

Re: Error while updating FMS master by tem.bat

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
The file extension is wrong ... C:\APLM\...\fsc\fmsmaster_FSC_AMWWSTEST_infodba.xml.orig. It should end in xml not orig?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error while updating FMS master by tem.bat

I have attached my error log.Please tell me the solution

 

*************************************************************************
**************************** INSTALL BEGINS *****************************
*************************************************************************
*************************************************************************
Time of Install: Wed Jul 06 12:32:55 IST 2016
Operating System: Windows Server 2008
OS Version: 6.1
User Name: infodba
User Home: C:\Users\infodba
Application: tceng
Application Version:8000.3.0.41
*************************************************************************
*************************************************************************
No debugging options are enabled
*************************************************************************
*************************************************************************
No defaults files are in use
*************************************************************************
Loading C:\APLM\Siemens\Teamcenter8\install\uninstall.xml
=====================================================
Processing <maintenance> feature FMS Server Cache
Time: Wed Jul 06 12:32:55 IST 2016
=====================================================
*** Processing block FMS Server Cache/maintenance:0
Running com.teamcenter.install.tceng.fms.fsc.Fsc
***
*** Running com.teamcenter.install.tceng.fms.fsc.Fsc
***
Updating master file
Copying file C:\APLM\Siemens\TEAMCE~1\fsc\fmsmaster_FSC_AMWWS056_infodba_01.xml to C:\APLM\Siemens\TEAMCE~1\fsc\fmsmaster_FSC_AMWWS056_infodba_01.xml.orig
Copying file C:\Users\infodba\AppData\Local\Temp\2\fmsmaster4718804445363511649.xml to C:\APLM\Siemens\TEAMCE~1\fsc\fmsmaster_FSC_AMWWS056_infodba_01.xml
An error occurred during execution. Stack trace follows...
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:131)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:106)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:140)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1098)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1043)
com.teamcenter.install.tem.struct.TcFeature.maintenance(TcFeature.java:825)
com.teamcenter.install.tem.director.actions.MaintenanceAction.execute(MaintenanceAction.java:30)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:111)
com.teamcenter.install.tem.director.Director.run(Director.java:53)
java.lang.Thread.run(Unknown Source)
***
*** CANCELLED
***
=====================================================
Installation interrupted due the following reason:

Processing <maintenance> of feature FMS Server Cache failed: com.teamcenter.install.util.struct.exceptions.FileMissingException: The path 'C:\Users\infodba\AppData\Local\Temp\2\fmsmaster4718804445363511649.xml' was not found.
Time: Wed Jul 06 12:33:17 IST 2016
=====================================================
Copying file C:\APLM\Siemens\Teamcenter8\install\configuration.xml to C:\APLM\Siemens\Teamcenter8\install\configuration1607061233.xml

Re: Error while updating FMS master by tem.bat

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The log shows that you are not able to either access the folder or the file...

Copying file C:\Users\infodba\AppData\Local\Temp\2\fmsmaster471​8804445363511649.xml to C:\APLM\Siemens\TEAMCE~1\fsc\fmsmaster_FSC_AMWWS05​6_infodba_01.xml
An error occurred during execution. Stack trace follows...

Check that C:\Users\infodba\AppData\Local\Temp\2 exists

 

Check that C:\Users\infodba\AppData\Local\Temp\2\fmsmaster471​8804445363511649.xml exists

Check that the user running TEM (run as administrator) is the owner of C:\APLM\Siemens\TEAMCE~1\fsc\fmsmaster_FSC_AMWWS05​6_infodba_01.xml

 

The path 'C:\Users\infodba\AppData\Local\Temp\2\fmsmaster47​18804445363511649.xml' was not found.

My best guess is that ...\Temp\2\ does not exist. You can create ...\Temp\2\ to resolve the issue.

 

 

How does \Temp\ get a 2 appended? That's another story about a windows feature which is automatically "checked" ootb and relates to "Use temporary folders per session". Basically, the session number is appended (which can change).


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error while updating FMS master by tem.bat

Thanks Randy for ur reply...
This issue is solved...I have just renamed the configuration.xml file with the old configuration file which ran successfully...
Thus trick clicked and now I am able to update FMS master...

Thanks friends for ur suggestion..


My another query left unsolved which is posted by me.. FCC ERROR.please give suggestion for that too
Regards,
Ganesh

Re: Error while updating FMS master by tem.bat

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I'm glad you were able to get the FMS Master updated using TEM. You should compare the "good" and "bad" configuration.xml files to see the difference and identify the root cause of the issue.

 

FCC ERROR has 4 responses and is awaiting your feedback.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4