Cancel
Showing results for 
Search instead for 
Did you mean: 

Error while upgrading TC 9.1.2.5 to TC 11.2.0 (plmxml_tm_edit_xsl)

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello.
I am getting the following error while upgrading from tc 9.1.2.5 to tc 11.2.0.
If you have any information to help, please answer.
Thank you.

 

image.pngimage.png

4 REPLIES 4
Highlighted

Re: Error while upgrading TC 9.1.2.5 to TC 11.2.0 (plmxml_tm_edit_xsl)

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Is there a log/syslog for plmxml_tm_edit_xsl in (new) TC_ROOT\logs\<datetime>\ and can you also attach TC_ROOT\logs\shell.err?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error while upgrading TC 9.1.2.5 to TC 11.2.0 (plmxml_tm_edit_xsl)

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I have attached the log/syslog file you requested.
Thank you for your interest in my problem.

 

below is shell.err

image.png

Re: Error while upgrading TC 9.1.2.5 to TC 11.2.0 (plmxml_tm_edit_xsl)

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I couldn't figure out why TEM was able to import files from previous commands but failed on this command. Obviously, the FSC was started and working correctly since previous commands imported files successfully. Then I thought it might be permissions on the new TC_DATA directory since that's where the XML lives.

The syslog shows the error:
ERROR - 2018/04/19-12:26:12.559 UTC - NoId - FileTickets::getFmsBootStrapUrls -- The preference Fms_BootStrap_Urls could not be found or has no values.

You'll need to change the Fms_BootStrap_urls value to include the http addresses of your FSC(s). How can you do that without logging into a 2tier? Use the command line utility "preferences_manager". The process will be to export the current value, make any changes, then import the new value.

Create a text file containing:
Fms_BootStrap_urls

In a (new) tc command window:
preferences_manager -u=infodba -p=infodba -g=dba -mode=export -scope=SITE -file=prefList.txt -out_file=C:\Temp\prefs.xml

Open C:\Temp\prefs.xml and add any values for the FSC(s) [Tip: Copy the address from FMS Master] and save the file.

preferences_manager -u=infodba -p=infodba -g=dba -mode=import -scope=SITE -file=C:\Temp\prefs.xml -action=OVERRIDE

Then retry TEM.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Error while upgrading TC 9.1.2.5 to TC 11.2.0 (plmxml_tm_edit_xsl)

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you for your help.
Fixed after correcting and importing preferences.