Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Error while upgrading TC9 to TC10/11 (fnd0inprocess)

Siemens Creator Siemens Creator
Siemens Creator

Hi Experts,

 

we face currently the problem with an upgrade process at the customer...

 

does anybody has an idea?

 

We think its something with the database (MS SQL Server 2012)

 

ODBC error. SQLSTATE: 42000 Native error: 9002
Message: [Microsoft][ODBC SQL Server Driver][SQL Server]The transaction log for database 'PLM1' is full due to 'ACTIVE_TRANSACTION'.
Approx SQL was "UPDATE PWORKSPACEOBJECT SET pfnd0InProcess = CASE VLA_38_7 WHEN 0 THEN 0 ELSE 1 END"
NOTE - 2018/12/06-09:25:47.849 UTC - NoId - ===>Took 24.185 seconds to execute that SQL (returning 0 rows) - Teamcenter.POM at D:\workdir\tc10171w1128_win64\src\foundation\pom\eim\eim_enquire.cxx(5722)
NOTE - 2018/12/06-09:25:47.849 UTC - NoId - That SQL took a long time to execute -- set TC_SLOW_SQL to -1.0 to suppress this analysis - Teamcenter.POM at D:\workdir\tc10171w1128_win64\src\foundation\pom\eim\eim_enquire.cxx(5801)

commit called with error set (Update fnd0InProcess attribute on WSO)
*** EIM_check_error: code 9002
NOTE - 2018/12/06-09:25:47.849 UTC - NoId - (EIM_trans_util) [Microsoft][ODBC SQL Server Driver][SQL Server]The transaction log for database 'PLM1' is full due to 'ACTIVE_TRANSACTION'. - Teamcenter.POM at D:\workdir\tc10171w1128_win64\src\foundation\pom\eim\eim_trans_util.cxx(4542)


#######inside EIM_not_ok##########

sqlca_error_code is 9002
EIM_db_error_code is 545001
ROLLBACK;

 

 

----------------------------------------------------------------------------
Executing command 29 of 158...
Section: post-schema-add
File: D:\plm\plm1root\tc10\install\foundation\upgrade_foundation_v20091.default
Command: migrate_wso_inprocess_attr -u=infodba -p=%TC_USER_PASSWD% -g=dba
----------------------------------------------------------------------------
Command start time: Do Dez 06 10:24:20 AM 2018
Output:


Fatal Error: Top level std::exception handler called. Caught exception: Use askUserMessage ( ) or askSyslogMessage ( )
Command end time: Do Dez 06 10:25:11 AM 2018
Command duration: 51.385 seconds
ERROR: Execution of command 29 failed


----------------------------------------------------------------------------
Executing command 29 of 158...
Section: post-schema-add
File: D:\plm\plm1root\tc10\install\foundation\upgrade_foundation_v20091.default
Command: migrate_wso_inprocess_attr -u=infodba -p=%TC_USER_PASSWD% -g=dba
----------------------------------------------------------------------------
Command start time: Do Dez 06 10:25:11 AM 2018
Output:


Fatal Error: Top level std::exception handler called. Caught exception: Use askUserMessage ( ) or askSyslogMessage ( )
Command end time: Do Dez 06 10:25:47 AM 2018
Command duration: 36.188 seconds
ERROR: Execution of command 29 failed

Upgrade end time: Do Dez 06 10:25:47 AM 2018
Upgrade duration: 3 minutes 16.202 seconds
ERROR: Upgrade failed.

3 REPLIES 3

Re: Error while upgrading TC9 to TC10/11 (fnd0inprocess)

Siemens Legend Siemens Legend
Siemens Legend

Your SQL server is having problems with disk space.

 

Do you have an MS SQL Server DBA at hand? They should look at this and perhaps change the DB transaction log settings.

Also, there's these:

 

https://support.industrysoftware.automation.siemens.com/docs/teamcenter/SQL_Server_for_Teamcenter_Be...

 

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&dt=faq&file_type=html&i...


Otherwise this might be of help:

https://stackoverflow.com/questions/17674973/the-transaction-log-for-the-database-is-full

Re: Error while upgrading TC9 to TC10/11 (fnd0inprocess)

Siemens Creator Siemens Creator
Siemens Creator

Thank you @TheGAP . We already changed this options after the first crash... still not working..

 

Could be there a problem with some "new" updates from the MS SQL Server? Maybe something important changed?

 

BR Luke

Re: Error while upgrading TC9 to TC10/11 (fnd0inprocess)

Siemens Creator Siemens Creator
Siemens Creator

Hi @TheGAP:

 

ok... after modifying it again and configured to "unlimited" it worked ! Thank you very much