Cancel
Showing results for 
Search instead for 
Did you mean: 

Export BOM by PLMXML

Experimenter
Experimenter

Good day.

 

I have a problem with plmxml export when I try to export an assembly's structure.

 

There is my assembly Assy-1:

 

13.PNG

figure 1

 

when I tap View->Unpack All. I see this:

 

14.PNG

figure 2

 

object det1 has 2 separate instance.

 

When I try to make PLMXML of Assy-1. Teamcenter exports structure with ths 2 separate instance of det1 (like in fig.2), but I need 1 instance of det1 with quantity 2 (fig. 1).

 

How can I do it?

 

ps. If you need plmxml, I can attach.

 

 

9 REPLIES 9

Re: Export BOM by PLMXML

Experimenter
Experimenter

Hi mjadmin,

 

What "Transfer Mode" are you using when exporting to PLMXML?

 

Something Default or Custom Built?

 

BR

TobbeP

Highlighted

Re: Export BOM by PLMXML

Experimenter
Experimenter

Hello, TobbeP

 

I use Custom Built rules. It includes some custom properties in property set and Closure rules

Re: Export BOM by PLMXML

Experimenter
Experimenter

Good Day. I solve my problem by adding some preffereces.
So if someone has the same problem, I can help

Re: Export BOM by PLMXML

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi mjadmin,

 

Can you tell me which kind of preference did you set to do it please ?

Re: Export BOM by PLMXML

Genius
Genius
yes, I would know the preferences.

Re: Export BOM by PLMXML

Hi , Kindly let me know what closure rule and preferences you have used

Re: Export BOM by PLMXML

Experimenter
Experimenter
Could you please attach plmxml? Thanks.

Re: Export BOM by PLMXML

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Can you please share the preferences you are used. Thanks.

Re: Export BOM by PLMXML

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

The preference to toggle packed/unpacked export is:

 

PLMXML_export_packed_bom_<transfer-mode-name>

You have to create one per transfermode that is to be exported as packed.

 

see https://docs.plm.automation.siemens.com/tdoc/tc/12/help/#uid:export_performance_improvement

 

 

Tricia Crichton | Software Architect | SEAL PLM, Inc