Showing results for 
Search instead for 
Do you mean 
Reply

Export "Saved Property Finder/Formatters"

Hi,

I would like to export 3 "Saved Property Finder/Formatters". There for I used:

  • plmxml_export -u=infodba -p=xxxxxx -class=ImanPFF -xml_file=d:\ff.xml, and
  • plmxml_export -u=infodba -p=xxxxxx -uid=CMLAAAEFIbZoUD -xml_file=d:\fff.xml

but both exports give me no usable data.

 

Is there a way to export this data?

 

Thanks,

 

Marcel

1 REPLY

Re: Export "Saved Property Finder/Formatters"

Hi,

Got this information from GTAC:

 

1. Build a TCXML Transfermode to export PFF as TCXML format 
a. Prepare a PropertySet named "PFF" with following properties: CLASS.ImanPFF:PROPERTY:PFF_class:DO CLASS.ImanPFF:PROPERTY:PFF_clauses:DO CLASS.ImanPFF:PROPERTY:PFF_desc:DO CLASS.ImanPFF:PROPERTY:PFF_name:DO 
	b. Prepare a Transfermode "TCXML_Export_PFF" with 
i. context "DEFAULT_TIE_CONTEXT" 
ii. Transfer type : Export 
iii. Schema: TCXML (not PLMXML) 
iv. PropertySet: PFF (just created) (Remark: No ClosureRules!) 
2. Exit from Rich Client 
3. In TC command prompt run command line: 
tcxml_export -u=infodba -p=infodba -g=dba -class=ImanPFF -file=C:\temp\all_PFF.tcxml -transfermode=TCXML_Export_PFF 
-- IMPORT -- 
4. Import it to another site as below: 
tcxml_import -u=infodba -p=infodba -g=dba -file=C:\temp\all_PFF.tcxml -transfermode=incremental_import 

HTH,

xtof