Cancel
Showing results for 
Search instead for 
Did you mean: 

FLEXlm License Error.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello ,
First of all i want to give information about the system.
Teamcenter : 11.2                                  Enviroment Variable is setted correctly.
NX:12                                                        Licence Version is 12
Java Version : 1.7                                   Client Machine : Admin
SPLM_LICENSE_SERVER:8.2.4        Server Machine : Gurkan-pc
The firewall is closed and i don't use any antivirus program.
I'm getting error that is FLEXlm Initialization failed while i try to login the TC on client machine or server machine. I checked the evr. variables, they look setted as correctly. Also i can ping (with name or ip) server from the client machine (there is no loss).In addition , when i check the lmtools to use Start/Stop/Reread License File features , i'm getting an errors you can see detailed inf. about the error according to the feature's names.

Stop - Unable to stop license server.
Reread License File - Reread Server Failed. (However , in the licence file is arranged according to the composite ID of server machine.)

Start- The server may already be running!!
I applied clean uninstall to SPLM_LICENSE_SERVER then i installed it again but it did not help to solve that problem.A week ago , there was no problem about that. Also i check the network changes but there was no change was applied for network.
Moreover , if you want to know more detailed please let me know. I will send to you splm_ugsmd.log file to check it.
How can i fix that problem ?

4 REPLIES

Re: FLEXlm License Error.

Phenom
Phenom

good afternoon,
judging by your log, some licenses require the creation and configuration of options file:

 
9:15:51 (ugslmd) NOTE: Some features are USER_BASED or HOST_BASED
 
9:15:51 (ugslmd) If a reread is done, and the INCLUDE list changes for these
 
9:15:51 (ugslmd) there is a delay of 12 hours for this to take effect.
 
9:15:51 (ugslmd)
 
9:15:51 (ugslmd) Licenses are case sensitive for ugslmd
 
9:15:51 (ugslmd)
 
9:15:51 (ugslmd) EXTERNAL FILTERS are OFF
 
9:15:51 (ugslmd) USER_BASED license error for CAR_ROBCAD (INCLUDE missing)
 
9:15:51 (ugslmd) Please ensure that no more than 10 users for CAR_ROBCAD
 
9:15:51 (ugslmd) are in an INCLUDE list in the daemon options file.
 
9:15:51 (ugslmd) To set up your options, modify the line:
 
9:15:51 (ugslmd) VENDOR ugslmd ... / ugslmd
 
9:15:51 (ugslmd) to read:
 
9:15:51 (ugslmd) VENDOR ugslmd ... / ugslmd <pathname> /ugslmd.opt
 
9:15:51 (ugslmd) where <pathname> is the directory where you place
 
9:15:51 (ugslmd) ugslmd.opt
 
9:15:51 (ugslmd) The options file should contain lines like this:
 
9:15:51 (ugslmd) INCLUDE CAR_ROBCAD USER <username>

I try to find and give you a link how to create it

Re: FLEXlm License Error.

Phenom
Phenom

Re: FLEXlm License Error.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Arthur ,

Thanks for helps , but i could not understand exactly why i should create the opt file. ? Could you explain more detailed ? If you helps to answer i can share the lic . file with you.

 

Best Regards

Gurkan

Re: FLEXlm License Error.

Phenom
Phenom

In your license file some features are USER_BASED and they require options file, I do not know whether you will use them or not, these are the features that have a USER_BASED license error in your log file, for example:

9:15:51 (ugslmd) USER_BASED license error for CAR_PLANTSIM_PROF (INCLUDE missing)

You have two options:

1) Cut these bundles from the license file
2) Configure options file