Cancel
Showing results for 
Search instead for 
Did you mean: 

FLEXnet Licensing error:-97,121

Experimenter
Experimenter

Hi,

 

When i am opening my teamcenter it shows me flexlm intialisation is failed. Due to this i checked in lm tools i am getting FLEXnet Licensing error:-97,121 this type error.

 

what i want to do know?

 

I am struggling with this error.

 

Kindly help me to sort out this error.

3 REPLIES 3

Re: FLEXnet Licensing error:-97,121

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
It is either a configuration error or a firewall issue. Open lmtools on the server (wherever the license is installed) and click the Config Services tab. Validate that all paths are correct (including the log). Then click Start/Stop/Reread, stop the license server, wait 30 seconds, and start the license server. Then click Server Status and click Perform Status Enquiry. If there is an error then copy/paste into this thread or you can attach the log.
If the license server starts without error then try disabling the firewall temporarily to test getting a license.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: FLEXnet Licensing error:-97,121

Creator
Creator

I'm having this error but the solution didn't work for me. I think there's an error with the Host ID or something.

 

Log file attached:

 

 

 9:04:46 (lmgrd) -----------------------------------------------

 9:04:46 (lmgrd)   Please Note:

 9:04:46 (lmgrd) 

 9:04:46 (lmgrd)   This log is intended for debug purposes only.

 9:04:46 (lmgrd)   In order to capture accurate license

 9:04:46 (lmgrd)   usage data into an organized repository,

 9:04:46 (lmgrd)   please enable report logging. Use Flexera Software LLC's

 9:04:46 (lmgrd)   software license administration  solution,

 9:04:46 (lmgrd)   FlexNet Manager, to  readily gain visibility

 9:04:46 (lmgrd)   into license usage data and to create

 9:04:46 (lmgrd)   insightful reports on critical information like

 9:04:46 (lmgrd)   license availability and usage. FlexNet Manager

 9:04:46 (lmgrd)   can be fully automated to run these reports on

 9:04:46 (lmgrd)   schedule and can be used to track license

 9:04:46 (lmgrd)   servers and usage across a heterogeneous

 9:04:46 (lmgrd)   network of servers including Windows NT, Linux

 9:04:46 (lmgrd)   and UNIX. Contact Flexera Software LLC at

 9:04:46 (lmgrd)   www.flexerasoftware.com for more details on how to

 9:04:46 (lmgrd)   obtain an evaluation copy of FlexNet Manager

 9:04:46 (lmgrd)   for your enterprise.

 9:04:46 (lmgrd) 

 9:04:46 (lmgrd) -----------------------------------------------

 9:04:46 (lmgrd) 

 9:04:46 (lmgrd) 

 9:04:46 (lmgrd) Server's System Date and Time: Tue Aug 28 2018 09:04:46 Hora de verano romance

 9:04:46 (lmgrd) pid 6636

 9:04:46 (lmgrd) SLOG: Summary LOG statistics is enabled.

 9:04:46 (lmgrd) Done rereading

 9:04:46 (lmgrd) FlexNet Licensing (v11.13.1.3 build 176543 x64_n6) started on Ingenieria-01 (IBM PC) (8/28/2018)

 9:04:46 (lmgrd) Copyright (c) 1988-2015 Flexera Software LLC. All Rights Reserved.

 9:04:46 (lmgrd) World Wide Web:  http://www.flexerasoftware.com

 9:04:46 (lmgrd) License file(s): C:\SEFlex\Program\SELicense.dat

 9:04:46 (lmgrd) lmgrd tcp-port 27001

 9:04:46 (lmgrd) (@lmgrd-SLOG@) ===============================================

 9:04:46 (lmgrd) (@lmgrd-SLOG@) === LMGRD ===

 9:04:46 (lmgrd) (@lmgrd-SLOG@) Start-Date: Tue Aug 28 2018 09:04:46 Hora de verano romance

 9:04:46 (lmgrd) (@lmgrd-SLOG@) PID: 6636

 9:04:46 (lmgrd) (@lmgrd-SLOG@) LMGRD Version: v11.13.1.3 build 176543 x64_n6 ( build 176543 (ipv6))

 9:04:46 (lmgrd) (@lmgrd-SLOG@) 

 9:04:46 (lmgrd) (@lmgrd-SLOG@) === Network Info ===

 9:04:46 (lmgrd) (@lmgrd-SLOG@) Listening port: 27001

 9:04:46 (lmgrd) (@lmgrd-SLOG@) 

 9:04:46 (lmgrd) (@lmgrd-SLOG@) === Startup Info ===

 9:04:46 (lmgrd) (@lmgrd-SLOG@) Is LS run as a service: Yes

 9:04:46 (lmgrd) (@lmgrd-SLOG@) Server Configuration: Single Server

 9:04:46 (lmgrd) (@lmgrd-SLOG@) Command-line options used at LS startup: -c C:\SEFlex\Program\SELicense.dat -l C:\SEFlex\Program\Debug.log -z -s 

 9:04:46 (lmgrd) (@lmgrd-SLOG@) License file(s) used:  C:\SEFlex\Program\SELicense.dat

 9:04:46 (lmgrd) (@lmgrd-SLOG@) ===============================================

 9:04:46 (lmgrd) SLOG: FNPLS-INTERNAL-VL1-4096

 9:04:46 (lmgrd) Starting vendor daemons ... 

 9:04:46 (lmgrd) Started selmd (pid 6644)

 9:04:46 (selmd) FlexNet Licensing version v11.13.1.3 build 176543 x64_n6

 9:04:46 (selmd) SLOG: Summary LOG statistics is enabled.

 9:04:46 (selmd) SLOG: FNPLS-INTERNAL-CKPT1

 9:04:46 (selmd) SLOG: VM Status: 0

 9:04:46 (selmd) SLOG: FNPLS-INTERNAL-CKPT2

 9:04:46 (selmd) Using options file: "C:\SEFlex\Program\selmd.opt"

 9:04:46 (selmd) Server started on Ingenieria-01 for:	solidedgeclassic 

 9:04:46 (selmd) server_id	

 9:04:46 (selmd) Wrong hostid on SERVER line for license file:

 9:04:46 (selmd) 	C:\SEFlex\Program\SELicense.dat

 9:04:46 (selmd) SERVER line says SE_HWKEY_ID=36243, hostid is SE_HWKEY_ID=14763

 9:04:46 (selmd) Invalid hostid on SERVER line

 9:04:46 (selmd) Disabling 1 license from feature server_id(087A 10F6 9906 1D48 )

 9:04:46 (selmd) Disabling 1 license from feature solidedgeclassic(16C6 943C 63EC 56D8 )

 9:04:46 (selmd) EXTERNAL FILTERS are OFF

 9:04:46 (selmd) Not logging UNSUPPORTED messages

 9:04:46 (lmgrd) selmd using TCP-port 49597

 9:04:46 (selmd) SLOG: Statistics Log Frequency is 240 minute(s).

 9:04:46 (selmd) SLOG: TS update poll interval is 600 seconds.

 9:04:46 (selmd) SLOG: Activation borrow reclaim percentage is 0.

 9:04:46 (selmd) (@selmd-SLOG@) ===============================================

 9:04:46 (selmd) (@selmd-SLOG@) === Vendor Daemon ===

 9:04:46 (selmd) (@selmd-SLOG@) Vendor daemon: selmd

 9:04:46 (selmd) (@selmd-SLOG@) Start-Date: Tue Aug 28 2018 09:04:46 Hora de verano romance

 9:04:46 (selmd) (@selmd-SLOG@) PID: 6644

 9:04:46 (selmd) (@selmd-SLOG@) VD Version: v11.13.1.3 build 176543 x64_n6 ( build 176543 (ipv6))

 9:04:46 (selmd) (@selmd-SLOG@) 

 9:04:46 (selmd) (@selmd-SLOG@) === Startup/Restart Info ===

 9:04:46 (selmd) (@selmd-SLOG@) Options file used: C:\SEFlex\Program\selmd.opt

 9:04:46 (selmd) (@selmd-SLOG@) Is vendor daemon a CVD: No

 9:04:46 (selmd) (@selmd-SLOG@) Is TS accessed: No

 9:04:46 (selmd) (@selmd-SLOG@) TS accessed for feature load: -NA-

 9:04:46 (selmd) (@selmd-SLOG@) Number of VD restarts since LS startup: 0

 9:04:46 (selmd) (@selmd-SLOG@) 

 9:04:46 (selmd) (@selmd-SLOG@) === Network Info ===

 9:04:46 (selmd) (@selmd-SLOG@) Listening port: 49597

 9:04:46 (selmd) (@selmd-SLOG@) Daemon select timeout (in seconds): 1

 9:04:46 (selmd) (@selmd-SLOG@) 

 9:04:46 (selmd) (@selmd-SLOG@) === Host Info ===

 9:04:46 (selmd) (@selmd-SLOG@) Host used in license file: Ingenieria-01

 9:04:46 (selmd) (@selmd-SLOG@) Running on Hypervisor: None (Physical)

 9:04:46 (selmd) (@selmd-SLOG@) LMBIND needed: No

 9:04:46 (selmd) (@selmd-SLOG@) LMBIND port: -NA-

 9:04:46 (selmd) (@selmd-SLOG@) ===============================================

 9:04:46 (selmd) No valid hostids, exiting

 9:04:46 (selmd) EXITING DUE TO SIGNAL 25 Exit reason 2

 9:04:49 (lmgrd) selmd exited with status 25 (Invalid host)

 9:04:49 (lmgrd) Please correct problem and restart daemons

 

Re: FLEXnet Licensing error:-97,121

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Your hardware key is incorrect for this license. You need a new key or a new license.

9:04:46 (selmd) SERVER line says SE_HWKEY_ID=36243, hostid is SE_HWKEY_ID=14763
9:04:46 (selmd) Invalid hostid on SERVER line

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4