Cancel
Showing results for 
Search instead for 
Did you mean: 

FMS Master

Genius
Genius

Hello

I need to define an FMS to connect with the master FMS. At the end of installation I get a TODO task to add a line in the fmsmaster file. I edited the fmsmaster file as shown in attached image but after changing Master FMS doen't start.

what is wrong with my configuration?

 

Thanks.

 

3 REPLIES 3

Re: FMS Master

Siemens Phenom Siemens Phenom
Siemens Phenom

it looks a little bit "wrong" ;-)

you entered your new fsc configuration in the middle of your first FSC defintion...

it would be better if it looks like this:

...

<fscgroup id="mygroup">

  <fsc id="FSC_sapplmTrain_Teamcenter" address="http://sapplm-train:4544" ismaster="true">

    <volume id="...." />

    <transientvolume id="..." />

  </fsc>

  <fsc id="FSC_SAPPLM_Administrator_1" address="http://sapplm:4544" ismaster="false"/>

  <clientmap subnet="127.0.0.1" mask="0.0.0.0">

   <assignedfsc fscid="FSC_sapplmTrain_Teamcenter" priority="0"/>

  </clientmap

</fscgroup>

...

Re: FMS Master

Genius
Genius

Thanks @MarkusK

 

Re: FMS Master

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
When your FSC service doesn't start or starts then stops within 5 seconds then make sure to review the logs for a clue as to why: TC_ROOT\fsc\FSC_*.stdout or stderr. Very useful for debugging.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4