Cancel
Showing results for 
Search instead for 
Did you mean: 

FQDN in TreeCache

Siemens Creator Siemens Creator
Siemens Creator

Using INSWEB to produce a tc.war file. The TreeCache cluster seems to be TRUNCATING after a certain # of characters.

Trying to add 2 new pool servers into the cluster (total of 8 now), but they never get generated in the war file. It appears that there are too many characters, since we started adding the Fully Qualified Domian Name (FQDN). Is there is a character Limitation using INSWEB for the TreeCache Field?   The field takes the characters, no problem, but the TC.WAR file doesn’t grab them.

 

1 REPLY 1

Re: FQDN in TreeCache

Siemens Creator Siemens Creator
Siemens Creator

 

Looks like INSWEB does not update WAR file automatically after a change has been made to the context parameters.  Shows as fixed in TC 11.5